PSoC™ Creator & Designer Forum Discussions
Dear All,
I am developing a relatively complex project and lastly the option of Debug is not active any longer, so I can not debug my project. I attach a picture of the PSOC Creator menus so you can understand what I am telling you.
Any idea where I should look for it and active it again? I have checked the PSOC Creator Manual but didnt find any related to this.
Thanks in advance,
Joaquin.
Show LessHello,
I just installed PSoC Creator 3.3 SP1. When I try to create a new project, starting from scratch, CY8CKIT-049-42xx is not part of the target hardware list. I only get several CYBLE modules. A configuration problem?
Beware: I'm a newbie...
Pascal
Show LessHello
I am trying to build a proxy sense application using a CY8CMBR3102.
Although what i find is that there is a lot of toggling on the output pin even when my hand is not near the sensor.
Although the above information is quite vague and incomplete, please bear with me till i lay hands on the programmer.
(The existing board is designed by someone else and he had programmed it, and i dont have his project file with me )
What i would expect from the community is some early guidance like few do's and don'ts , or some information sharing regarding kick-starting the development with this part.
If you can share anything please do..
i will be back with some more info later
Show LessHi all,
We have a different behaviour of the Cypress SPI modules on different Cypress CPUs.
When we use the SPI Slave non SCB (UDB?) based, version 2.70 on a CY8C4247LQI-BL483 we do receive SPI frames
from a Renesas controller, means the buffersize remains 0,
but when we change to CYBL10563-56LQXI we can only use the SCB based SPI module version 3.0 and
do not receive any frames with this component.
We use mode Slave and submode Motorola, with SCLK mode CPHA=1 and CPOL=0, Oversampling=8,
RX/TX data bits=8, MSB First, Number of SS:1, Active Low, with a FIFO Buffer size of 8 bytes. The datarate is 1kHz.
And the SCB SPI component has no rx/tx interrupt? Only an SPI_Done status and the various FIFO status and the buffer size?
Has anyone an idea why the modules are so different?
Thanks a lot and best regards
Andreas
Show LessHi,
Just Setting up CY8CKIT042BLEKIT, and I am getting the following PSoC Programmer error (Cut & past):
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
| KitProg Version 2.10 Firmware Update Finished at 2:34:59 PM
|
| FAILED! Failed at BlockID = 40 SubPkt = 0 Msg = The data is not of the proper form.. Please replug KitProg.
| Upgrading...
| Initializing... Firmware Upgrade Started at 2:34:48 PM
| Firmware Upgrade Requested at 2:34:48 PM
|
| Please navigate to the Utilities tab and click the Upgrade Firmware button Port Opened with Warnings at 2:33:28 PM
| KitProg version Expecting 2.14, but found 2.10. Opening Port at 2:33:27 PM
| Device set to CY7C65215-32LTXI at 2:33:27 PM
32768 FLASH bytes Device Family set to CY7C65210 at 2:33:27 PM
| Active HEX file set at 2:33:26 PM
|
|
| Users must be aware that the following PSoC device should not be powered or programmed at 5V. Doing so will cause damage to the device: CYRF89xxx
Session Started at 2:33:26 PM
| PPCOM Version 20.0
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Everything has been updated. CySmart and initial H/W demo works.
Thanks!
Bob
Here is another display component, this time for OLEDs using the WS0010 controller in 4-bit parallel mode. I tried to make it a drop-in replacement to the stock character LCD component, it should be pretty easy to use.
These modules are gorgeous! Really sharp with great viewing angles and available in various colors. I included a photo below of the module running with a PSoC5LP prototyping kit.
The component is available at my Github repository over here. I included a 'datasheet' with the component with info on how to use it, you can also check this blog post for more info.
Show LessI'm starting my first project with PSoCEVAL1 board. I try to replicate the example code which I found from the youtube video. Here I have attached the screen shot of the PSoC designer. The error says the "memory.inc" file is missing with the red cross mark. I don't know how to resolve the problem. Please help me to solve this problem.
My system configuration,
Windows 7 (64Bit), PSoC designer 5.4 (latest)
Udhay
Show LessI am working on psoc 1 based application program of cypress - on pulse oximeter(spo2) AN2313, but constantly facing same issue in pulse error, the probe I am using is a pulse oximeter probe from biometric cable with db9 connector, even tried with red led and ir , photodiode on breadboard circuit, still same problem, does not display spo2 value.
Show LessI have been working for a year with the PSOC creator. But also I have worked with a C++ IDE called Code Blocks. I have to say that it is less comfortable using PSOC creator because of the little details that could be added to it which already exists in CodeBlocks. small details such as I have to only open a single bracket after an if condition and the program immediately finishes the other bracket and the semicolon.