PSoC™ Creator & Designer Forum Discussions
hi every one ^^
i try to calculate the frequency of an input Pulse signal, sow i add a counter, the signal that i want to measure is a signal 200hz, 5ms, sow i add a clock 24mhz and try to count every 1mz for having the numer of impulse on
dont khnow why it dosnt work, need some help
thank u
Show LessDear community,
i'm very new to cypress psoc and have developed a little application which reads the temperature and humidity from an dht-22 sensor.
This works really great, but now i thought it would be much better to create an component as an easy driver source for future projects.
So what i've done til now is created an Library Project and added an symbol with one output pin (DHT-22 works with an single line data).
Then i created an api file .c and .h For read and write i created an schematic with an Terminale and an control register. The control register is used to read and write the data.
My problem now is that the Register seems to be optimized and is greyed out in my project.
Is my approach right? Or should things be done in an other way?
Regards
Moritz
Hi Cypress Team,
I have CY8C3246LTI-149 PMON connected to more than 5 to 6 voltage rails for monitoring in my Board and due to some issues, all the voltage rails shuts down exactly after 1 sec and reboots.
I want to check the voltage at PMON while the Board is powered ON state. Is it possible to monitor the LIVE voltage using this IDE?
Thx,
Sundar
Show LessWorking on some changes and suddenly the debugger always stops here ->>>, but there are no breakpoints set:
void cyfitter_cfg(void) { /* Disable interrupts by default. Let user enable if/when they want. */ CyGlobalIntDisable; /* Enable the clock in the interrupt controller for the routed interrupts */ ->>> CY_SET_REG8((void *)CYREG_UDB_UDB_INT_CLK_CTL, 0x01u);
There are no warnings, so I have no idea what I changed to cause this. Are there other reasons the debugger would trap, and how can I isolate them?
Show LessHello, I'm using CY8CKIT-042 PSoC Kit for my project but now when I open Psoc Creator it is showing me continuously one error i.e. warp synthesis not found. I'm attaching error image with this. So please help me to solve this error I even tried to uninstall and reinstall the software but till now no luck.
Show LessHi, todat I opened a new project, I wanted to have a timer running free on my project so I can need to get delta time, the thing is that I start the timer and it it counting backwards?? , how can I fix this?, It can not be a software Error, because I am Only calling Timer_Start(); and Timer_ReadCounter();
Thanks 😃
Show LessThe attached project can be built if the links between XxDMA and XxDMAB are removed. But if the 3 chain links are added, it fails to place some of the USB DMA. It will also build if many of the TxDMA_X is disabled.
I'm not using all the DMAs - what is the problem?
Error message:
Error: plm.M0046: E2806: Failed to place fixed-function blocks. See the report file for details.
Error: plm.M0046: "C:\Program Files (x86)\Cypress\PSoC Creator\4.0\PSoC Creator\bin/sjplacer.exe" failed (0xFFFFFFFF)
From the Report File:
Show Less<CYPRESSTAG name="Digital Placement">
Error: plm.M0046: E2806: Failed to place fixed-function blocks. See the report file for details.
"C:\Program Files (x86)\Cypress\PSoC Creator\4.0\PSoC Creator\bin/sjplacer.exe" --proj-name "Temp" --netlist-vh2 "Temp_p.vh2" --arch-file "C:\Program Files (x86)\Cypress\PSoC Creator\4.0\PSoC Creator\dev/arch/p4_udb2x4.ark" --rrg-file "C:\Program Files (x86)\Cypress\PSoC Creator\4.0\PSoC Creator\dev/psoc4/2/route_arch-rrg.cydata" --irq-file "C:\Program Files (x86)\Cypress\PSoC Creator\4.0\PSoC Creator\dev/psoc4/2/irqconn.cydata" --drq-file "C:\Program Files (x86)\Cypress\PSoC Creator\4.0\PSoC Creator\dev/psoc4/2/triggerconn.cydata" --dsi-conn-file "C:\Program Files (x86)\Cypress\PSoC Creator\4.0\PSoC Creator\dev/psoc4/2/dsiconn.cydata" --pins-file "pins_124-VFBGA.xml" --lib-file "Temp_p.lib" --sdc-file "Temp.sdc" --io-pcf "Temp.pci" --outdir .
<CYPRESSTAG name="Detailed placement messages">
I2807: The following instances could not be placed: \USBFS:ep3_dma\, \USBFS:ep4_dma\, \USBFS:ep6_dma\, USBOutDMA, USBInDMA
DMA placement:
DMA 0: <empty>
DMA 1: <empty>
DMA 2: TxDMAB_1
DMA 3: TxDMAB_0
DMA 4: <empty>
DMA 5: <empty>
DMA 6: <empty>
DMA 7: <empty>
DMA 8: RxDMAB_1
DMA 9: RxDMAB_0
DMA 10: TxDMA_1
DMA 11: TxDMA_0
DMA 12: RxDMA_1
DMA 13: RxDMA_0
DMA 14: \USBFS:ep1_dma\
DMA 15: \USBFS:ep2_dma\
DMA 16: <empty>
DMA 17: <empty>
DMA 18: <empty>
DMA 19: <empty>
DMA 20: <empty>
DMA 21: <empty>
DMA 22: <empty>
DMA 23: <empty>
DMA 24: <empty>
DMA 25: <empty>
DMA 26: <empty>
DMA 27: <empty>
DMA 28: <empty>
DMA 29: <empty>
DMA 30: <empty>
DMA 31: <empty>E2806: Failed to place fixed-function blocks. See the report file for details.
</CYPRESSTAG>
Hello,
First off, thanks for adding the export to Makefile option to PSoC Creator 4.0. It's a greatly needed feature that enables tons of new tooling for PSoC project code.
However, I've encountered some bugs that I'd like some assistance with. I'll add each bug as a separate reply to this post.
Show LessHi,
Just finished my first project. I feel confident with the software but I don't know how to create a standalone executable. ATM I have to attach the usb programmer for the uploaded program to boot and run. Have tried changing the project build options from debug to release but that didn't change anything. Simple question I know so I appreciate anyone who takes the time to reply. Have tried looking through the documentation and google but obviously not looking in the right place.
Thanks.
Show LessHow can I find the latest version of the KEES component library?
I have only 04/17/2014
from https://github.com/LagunaMatada/GlowTime
And how to update/Separate its components?