PSoC™ Creator & Designer Forum Discussions
The miniprog3 cy8ckit-002 I just bought can burn the program yesterday, but it can't burn today
Who can tell me what the problem is
The following is a screen capture
Show Less
Hi,
it seems that there's an update to PSoC Creator. However, the Cypress Updater throws an error message "Error:002, installer unable to download installation packages, the remote server has returned an error, 404 not found."
I'm facing this problem on two installations.
Anyone else having this issue?
Regards,
Ralf
Show LessWe are running Creator 4.1 and didn't upgrade to 4.2 because of existing program compatibility problems. Some kits, such as CY8CKIT-042-BLE want 4.2 at install. Any way to get them running with 4.1? Could not install both Creator 4.1 and 4.2 - had to remove one to install other.
Show LessMy first time using a graphic LCD, be gentle.
In the data sheet for the GraphicLCDIntf, it specifically lists about 7 display driver chips that it's compatible with.
In my initial searching for an LCD panel, I don't see any of those controller chips.
So what about parts like NT7108C, ST7565P, and ST7541? Is there a comprehensive list of controllers that this component is compatible with?
While I'm here, I'm having trouble finding a small, square, blue display. Like 160x160, around 2" diagonal. Any suggestions, I'm open.
Thanks in advance -
Dan
Show LessWe are considering PSoC4M.
And using MiniProg3 to write to the device.
Our system is +5V only.
Therefore, the target device setting to +5V will not recognize the device.
If it is set to + 3.3 V, it will operate normally.
So we confirmed the SWD IF at +5V,
VTARG/VDDD/VDDA : +5V
VDDIO : +5V
SWDIO : +3.3V peak Square wave
SWDCLK : +3.3V peak Square wave
The above operation was also the same with CY8CKIT-046.
However, CY8CKIT-046 operates normally even at target voltage setting +5V.
Is this SWD operation correct when setting the target voltage +5V?
I am in trouble because I can not find the difference between the designed board and the demo kit.
Reagards,
Masashi
Show LessHi,
I use PSOC creator to design schematic, I want to check correction for the logic sequence of node, is there any tool like logic simulator that could show the logic level diagram?
Chris
Show LessHow do I create test cases for USB to AHB model using PSoC ?
How or where do I find 'kit packages' to install for Creator?
ie, for the CY8CKIT-049-42xx
When I run Creator (3.0), under the Examples and Kit bar, it shows "No kit pacakges installed"
Show LessI use psoc creaor 4.2 ,and use find code example , when i searched the code ,and the document did not show ,and will crash ,the psoc creator will quit
Show LessI installed the latest update and tried to use the USB Configurator. I get this error and I don't see it installed on my PC. How do I install it?
Menu item action, Launch USB Configurator, failed. File not found 'C:\Program Files (x86)\Cypress\PDL\3.0.4\tools\win\usbdev-configurator-1.0\usbdev-configurator.exe'
Show Less