PSoC™ Creator & Designer Forum Discussions
Hello,
It seems that in the current revision of AN68272 the example project for a C# UART Host Flasher has disappeared. In other threads (e.g. UART bootloader host project in VC++ ), it is clearly stated that it once existed. I am wondering if Cypress removed that project intentionally and if so, why? Could someone give me an old revision of the project?
Thanks in advance.
Hi all,
For my project, I require to store values form an ADC into some variable. I am kinda new to C so I do not really know how datatypes work. I am trying to implement a PID controller, and from what i have read, the math is better done in 16 to 32 bits, however, the SAR ADC cannot go above 12 bits. Is there a way to change a uint8_t variable into a uint16_t? Or is there any other way around it.
Show Less新安装软件,不能找到此文件。
Hello
We have CY8CKIT-001 kit, where we are doing USB communication using USBFS using PSoC5LP Moadule. Now we want to give data to wavedac where pointer should directly point to EndPoint EP1 of USB communication . How to point directly to Endpoint RAM.
Show LessI know how to download code to a Cypress chip that is on an evaluation board connected to a Pioneer kit. I simply go through PSoC Creator.
How do I download code to, say, a CYBLE-022001-00 that is not on an evaluation board?
With NXP chips I use a PEMicro Cyclone and a custom-made connector.
Show LessHi all,
I have already posted about this before but here we go again. I have recently uninstalled psoc creator 4.2 and tried to re install it. Whenever the installation reaches the PSoC Programmer stage and the Clock Programmer stage, it tells me that there is a newer version already installed.
I already searched the registry and could not find anything else about it. It still gives me the same error and I cannot find these programs that are apparently already installed.
P.S the weird part is, the latest version of the clock programmer I could ind is the 1.8, so it would not sense for there to be a newer version already installed right?
Show LessHi all,
I deleted my previous version (4.1) to make space to download PSoC Creator 4.2. Long story short, after deleting 4.2 (Another Mistake), I tried to re-download it onto my computer, however. it kept giving me the following error:
It appears as if it stops once it tries to install the clock programmer (Correct me if I'm wrong), however, I cannot fins another version installed on my computer and it keeps giving me the same error every time I try to download it. Please help, It is driving me crazy.
Show LessThe miniprog3 cy8ckit-002 I just bought can burn the program yesterday, but it can't burn today
Who can tell me what the problem is
The following is a screen capture
Show Less
Hi,
it seems that there's an update to PSoC Creator. However, the Cypress Updater throws an error message "Error:002, installer unable to download installation packages, the remote server has returned an error, 404 not found."
I'm facing this problem on two installations.
Anyone else having this issue?
Regards,
Ralf
Show LessWe are running Creator 4.1 and didn't upgrade to 4.2 because of existing program compatibility problems. Some kits, such as CY8CKIT-042-BLE want 4.2 at install. Any way to get them running with 4.1? Could not install both Creator 4.1 and 4.2 - had to remove one to install other.
Show Less