cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

Anonymous
Not applicable

 This sounds silly, but i cannot find the Cypress USB Serial Drivers for Mac anywhere on google.

   

I am using the Psoc 4 Pioneer kit, i can detect the USB serial under windows, but i have no idea where the Mac drivers are. I need to send data over to a Mac.

   

Can anyone point me where to get the USB drivers please?

   

 

   

 

   

Thanks

0 Likes
6 Replies
ETRO_SSN583
Esteemed Contributor

Drivers here -

   

 

   

www.cypress.com/     USB SDK kits

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 Hi Dana,

   

I follow the instructions, copied the dylibs and the conf files, but when i plug in the usb, i still cant detect it as a serial port. What else needs to be done to detect it as a serial port?

0 Likes
ETRO_SSN583
Esteemed Contributor

If using a Pioneer card then you would have to use UART in PSOC 4 to com to

   

MAC. If you sue the PSOC 5LP on the board you could do a USBUART approach.

   

If former you would need RS232 interface chip like MAX232 to do the PC interface.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 Hi Dana,

   

 

   

I am using the 5LP on the board, and connecting to psoc 4 tx rx to the 5LP rx tx. Under windows i am able to detect it as a serial COM port. So i think MAC doesnt recognize it because it doesnt have the drivers. this is the USB UART approach right?

0 Likes
Anonymous
Not applicable

I still cant find the mac drivers for using the 5lp on the board as a serial device, anyone can help?

0 Likes
ETRO_SSN583
Esteemed Contributor

Consider filing a CASE -

   

 

   

To create a technical or issue case at Cypress -

   

 

   

www.cypress.com

   

“Support”

   

“Technical Support”

   

“Create a Case”

   

 

   

You have to be registered on Cypress web site first.

   

 

   

Regards, Dana.

0 Likes