cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

ETRO_SSN583
Esteemed Contributor

Build this into Creator as a tool, takes 2 R's and user has a

   

level translator w/o using an OpAmp and a fixed reference to do it.

   

 

   

Do not just incorporate the attached, build it into the IDE, and select

   

from standard R 1% values and compute worst case.

   

 

   

Regards, Dana.

0 Likes
1 Reply
rotec_264361
New Contributor II

There should be a section for Creator features here in the forum.

   

Any plans from Cypress?

0 Likes