cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

Anonymous
Not applicable

Hi, Psoc creator crashes randomly (but often) on my PC (Windows 10 home v 1803)

It seems to crash when it's opne and I'm not using it. There is no error message.

In the application journal, I've found :

------------------------

Nom de l’application défaillante psoc_creator.exe, version : 0.0.0.0, horodatage : 0x5a85e2fd

Nom du module défaillant : ucrtbase.dll, version : 10.0.17134.1, horodatage : 0xbb0923b6

Code d’exception : 0xc0000409

Décalage d’erreur : 0x000a273b

ID du processus défaillant : 0x3120

Heure de début de l’application défaillante : 0x01d4148027105cb3

Chemin d’accès de l’application défaillante : C:\Program Files (x86)\Cypress\PSoC Creator\4.2\PSoC Creator\bin\psoc_creator.exe

Chemin d’accès du module défaillant: C:\WINDOWS\System32\ucrtbase.dll

ID de rapport : 66705999-2373-4da2-a1b8-90a6914c940c

Nom complet du package défaillant :

ID de l’application relative au package défaillant :

--------------------

and each time, it's the same crash report. I've tryed to reinstall .NET framework (v4.7.2), but this has no effect.

I've only one version of Psoc creator installed on this PC (i've changed quite recently my PC).

Thanks for any help.

0 Likes
1 Solution
AnkitaS_51
Employee

Please check if you are trying to open Visual Studio and PSoC Creator simultaneously, then only is this error is occurring

This error is specific to Windows as evident from these links:

1)https://answers.microsoft.com/en-us/windows/forum/windows_10-files-winpc/ucrtbasedll-is-causing-my-a...

2)https://answers.microsoft.com/en-us/windows/forum/windows_10-performance/running-specialized-softwar...

View solution in original post

0 Likes
2 Replies
Anonymous
Not applicable

Hi,

I've checked those threads

"

This issue has been answered on other threads, links provided below:
1) PSoC Creator 4.0 Slow, Crashing

2) PSoc Creator 4.0 freezes several times also at the 4th PCs"

but this does not help me of fix the isse. I've also launched the .net repair tool.

Also, I've visual studio community 2013 also always open on my PC, I don't know if there could be a link, but visual studio is open in my case.

0 Likes
AnkitaS_51
Employee

Please check if you are trying to open Visual Studio and PSoC Creator simultaneously, then only is this error is occurring

This error is specific to Windows as evident from these links:

1)https://answers.microsoft.com/en-us/windows/forum/windows_10-files-winpc/ucrtbasedll-is-causing-my-a...

2)https://answers.microsoft.com/en-us/windows/forum/windows_10-performance/running-specialized-softwar...

View solution in original post

0 Likes