cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

Anonymous
Not applicable

Hello everybody,

   

I made a script that will open a project with the version of PsocCreator that it was created with (if available on the system).
This is functionality that I found very much lacking in PsocCreator. It is probably comparable to "Version Selector" from visual studio.

   

https://github.com/mjmlvp/LaunchPsocCreator

   

If there are issues, or you have pull requests please let me know. Any feedback could make the scripts more useable for general use.

   

 

   

Also, if cypress likes to make it part of the distribution in any form, I would love that.

   

Regards,

   

Martijn

0 Likes
1 Reply
cadi_1014291
Valued Contributor

Hi,

   

Thanks for the script, useful when having multiple versions of Creator installed on the PC.

   

Carlos

0 Likes