cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

Anonymous
Not applicable

Hi,
Just Setting up CY8CKIT042BLEKIT, and I am getting the following PSoC Programmer error (Cut & past):
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
| KitProg Version 2.10 Firmware Update Finished at 2:34:59 PM      
|
| FAILED! Failed at BlockID = 40  SubPkt = 0 Msg = The data is not of the proper form.. Please replug KitProg.
| Upgrading...
| Initializing... Firmware Upgrade Started at 2:34:48 PM
| Firmware Upgrade Requested at 2:34:48 PM    
|
| Please navigate to the Utilities tab and click the Upgrade Firmware button Port Opened with Warnings at 2:33:28 PM     
| KitProg version Expecting 2.14, but found 2.10. Opening Port at 2:33:27 PM                  
| Device set to CY7C65215-32LTXI at 2:33:27 PM
32768 FLASH bytes Device Family set to CY7C65210 at 2:33:27 PM
| Active HEX file set at 2:33:26 PM           
|
|
| Users must be aware that the following PSoC device should not be powered or programmed at 5V. Doing so will cause damage to the device: CYRF89xxx
Session Started at 2:33:26 PM               
| PPCOM Version 20.0
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Everything has been updated. CySmart and initial H/W demo works.
Thanks!
Bob
 

0 Likes
1 Solution
Anonymous
Not applicable

Solved.  Apparently you have to select the KitProg before you “Please navigate to the Utilities tab and click the Upgrade Firmware button”.

   

Bob

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

Solved.  Apparently you have to select the KitProg before you “Please navigate to the Utilities tab and click the Upgrade Firmware button”.

   

Bob

View solution in original post

0 Likes