Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

 I am working on a design in Creator 3.0 using a PSOC5LP that uses internally generated 60MHz clock or clocks.

   

(3.7V on all Vdds and 0-85/125 temperature range.)

   

Occasionally the Static Timing Analysis, under Clock Summary says the maximum frequency for a certain clock is a NEGATIVE NUMBER!

   

What does this mean, other than it does not like the design?

   

Thanks, Bill

   

PS: Is there a design recommendations document that addresses things like whether it is better to use one clock or multiple clocks of the same frequency? Or best methods for preventing hold time violations? I seem to get inconsistent or counter-intuitive results when I try simplifying my logic with the Static Timing Analysis.

0 Likes
1 Reply
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Double post, please follow up here www.cypress.com/

   

 

   

Bob

0 Likes