Announcements
IMPORTANT: Cypress Developer Community currently doesn’t allow sign-in to prepare for the upcoming transition. To learn more, check out our announcement.
cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

user_284076
New Contributor II

Error in customizer for component "PWM_v2_40" : EditParams : (Font 'Arial' does not support style 'Regular'.).

   

message apear on the screen when I double click on the pwm component to configure it.it works with my old "creator 2.0  " but not working with  "creator 2.1 sp1"

0 Likes
3 Replies
Bob_Marlowe
Expert II
        This looks a bit like a windows problem and an overwritten font-definition...   
   
Bob   
0 Likes
user_284076
New Contributor II

can u guide me to solve this problem ? I upgraded to creator 2.2 same problem is there ..now i am using creator 3 but same problem is there ..I am not sure about its windows problem or componet setting did not match with any setting out there...but what shoul I do to solve these problem..any suggestion will make it easy for me...thanks...

   

i attached snapshot of error on my screen

0 Likes
Anonymous
Not applicable
        Hi love232   
How was customize this module?   
If you could revert into default style, It might be solve.   
Is it happen on default PWM module?   
0 Likes