Creator warning: "apr.M0002:Analog signal ... is connected to one terminal only."

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

 When I compile my project with PSoC creator 3.0,there are notes that may indicate some problems:

   

"apr.M0002:Analog signal ... is connected to one terminal only."

   

The signal is internal to the ADC.

   

Will it affect the project's functionality? 

   

Ans:

   

This will not cause any issues with the functionality. There is a mux before Del-Sig ADC to select between the internal and external reference. Since we are using only the internal reference, one input to the AMux will be left unconnected.

   

Hence, it shows that analog signal is connected to only one terminal.

   

This will be corrected in the future versions of the component.

   
        
0 Likes
1 Solution
Roy_Liu
Moderator
Moderator
Moderator
5 comments on KBA First comment on KBA 10 questions asked

This note is considered as required, so no change is planned to be implemented.

Roy Liu

View solution in original post

0 Likes
5 Replies
Anonymous
Not applicable

Hello,

   

This still has not been corrected.  The Del-Sig ADC component still reports this note

   

Regards,

   

Ron

Roy_Liu
Moderator
Moderator
Moderator
5 comments on KBA First comment on KBA 10 questions asked

This note is considered as required, so no change is planned to be implemented.

Roy Liu
0 Likes
Anonymous
Not applicable

This will not cause any issues with the functionality. Contoh Lamaran Kerja There is a mux before Del-Sig ADC to select between the internal and external reference.

0 Likes
JoBr_1593366
Level 5
Level 5
100 sign-ins 50 questions asked 100 replies posted

This still happens in PSoC Creator  4.2 (4.2.0.641) with ADC_DelSig v3.30

0 Likes

It also happens with the Sequencing SAR ADC for PSoC 5LP in Creator 4.2 (4.2.0.641)