cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

Anonymous
Not applicable

Upgraded from Creator 4.0 to 4.1.

Several components had to be downloaded.

Uart was one of them.

However, I have several Uarts instanced, but only one gives this error during clean/build

Title: PSoC Creator Error prj.M0072

Unable to add "Uart_xxx" to "PSoC5". (An item of that name already exists.) ...

The same project under 4.0 has no such issues.

0 Likes
1 Solution
Anonymous
Not applicable

Yes, renaming didn't help.

What did finally fix it is to REMOVE the uart. Build.

Then add it back in.

GR

View solution in original post

0 Likes
3 Replies
AnkitaS_51
Employee

Have you tried renaming that UART component with the error.Can you provide us your project in PC4.0

0 Likes
Anonymous
Not applicable

Yes, renaming didn't help.

What did finally fix it is to REMOVE the uart. Build.

Then add it back in.

GR

View solution in original post

0 Likes
pacr_284376
Contributor

I got a similar problem :

* But not with UART but and I2C component I named TWI

Solved it by removing the Generated_Source folder.

More Background information :

- The reason was probably that I renamed this component from 'Twi' to 'TWI'. The directory in the Generated_Source also was still called 'Twi'. After removing the Generated_Source folder everything worked and the dir is now called 'TWI'.

- This TWI component is located inside a library I wrote  but that has probably nothing to do with it

- Using PSoC Creator 4.1 Update 1

- Sorry I have the error-generating project version not available

0 Likes