Creator Device P/N not synced to component catalog

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Here is an example where customer placed a DFB and an OpAmp, neither of

   

which is available for chosen part number.

   

 

   

    

   

          http://www.cypress.com/?app=forum&id=2233&rID=99512

   

 

   

Creator component selector should show ALL PSOC components, but ones

   

not available to specific part chosen should be grayed out.

   

 

   

Regards, Dana.

0 Likes
1 Reply
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Since there are so many cases to look for (what happens when the component is a macro that embedds one of these, and what to do when this depends on the configuration of the part?), this will get difficult. Also, one might change the part later on.

   

I would suggest to at least improve the error message to more clearly state what the problem is (though I think that 'Maximum number of Opamp Fixed Blacks exceeded' is quite precise). Maybe something like 'select a part with more Opamps'...

0 Likes