Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
PrMa_264311
Level 3
Level 3
First like received

 Just encountered a strange problem. I took a project from 2.2 SP1 and imported it into 3.0. I can compile and execute the code just fine in Debug mode. However, when the code is compiled in release mode, it fails to execute. In other words, the processor appears to hang. This is on a CY8C4125.

   

 

   

I did not have this issue in 2.2 SP1.

   

 

   

Thoughts?

0 Likes
4 Replies
Anonymous
Not applicable
        Hi Manjagu   
Which part was in failing ?   
Can you identify it ?   
Did you make some special setting for Build ?   
   
When I test in Release mode, same fail does not happen ever.   
However, it is 8C4245   
0 Likes
PrMa_264311
Level 3
Level 3
First like received

 It's a bit difficult to determine why the program has failed because all communications cease. The chip is a CY8C4125.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked
        I would suggest you to IMMEDIATELY create a "MyCase" (Support&Community->Technical Support -> Create a MyCase) and submit a complete project workspace created with Creator (File -> Create Workspace Bundle)   
   
Bob   
0 Likes
PrMa_264311
Level 3
Level 3
First like received

 Have done. Will see what they say. Thanks.

0 Likes