cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

VlYe_281166
New Contributor II
0 Likes
4 Replies
VlYe_281166
New Contributor II
    PSoC Creator  2.2 (2.2.0.293)   
   
    Culture: Russian (Russia)   
   
    OS Version: Microsoft Windows NT 6.1.7601 Service Pack 1   
   
    CLR Version: 2.0.50727.5466   
   
        
   
    Anybody have an Idea why?   
0 Likes
HeLi_263931
Honored Contributor II

You might want to test with an accuracy greater than 0%, or maybe switch to specify ppm. I tested it on an english Windows XP/SP3, and it worked there without problems.

0 Likes
HeLi_263931
Honored Contributor II

You can also try to file a support request, this might get you better help with that (since it seems that it a bug, not something you did wrong).

0 Likes
EvPa_264126
Valued Contributor II

Привет Kabron!
I created an empty project on two PC (Win7 64 and 32 Russia):
File--->New--->Project...
Design ----> Empty PSoC 5 Dessign
I changed the settings of  XTAL only.
Anything else?
Evgeniy (yhnm)

0 Likes