Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
MaLe_297531
Level 2
Level 2
10 sign-ins 5 replies posted First like received

I have the CY8CKIT_040 kit. This is the one that changes LED color and brightness via a 5x6 touchpad. I can't get some of the example Capsense projects working that ship with kit. The limited success I have had includes blinking the LED and getting the touchpad to control the 3-color LED. What I really need is to is display any data on the tuner or the Bridge Control Panel. Does anyone some example CapSense projects that work with this kit that use I2C and UART with the Bridge Control Panel?

   

Even a simple project that increments an interger and displays the current vlaue in the bridge control panel would be helpful for the CY8CKIT-040 kit.

0 Likes
3 Replies
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

I presume these are the projects you have been working with,

   

in Creator example projects -

   

 

   

   

 

   

Also here -    

   

          http://www.element14.com/community/docs/DOC-67927/l/psoc-4000-pioneer-development-kit#downloads

   

 

   

Possibly post a [project archive of one that does not work for forum to

   

look at -

   

 

   

    

   

          

   

“File”                                                             Creator

   

“Create Workspace Bundle”

   

 

   

Regards, Dana.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

These are PSOC 4 projects, possibly one that you could adapt -

   

 

   

    

   

          

   

 PSOC 4 element14.com

                                           
                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                  

S No

Date

Project Title

1

01-May-2013

Simple Blinking LED

2

02-May-2013

CapSense Slider Example

3

03-May-2013

PSoC 4 Pioneer Kit Annotation Library

4

06-May-2013

USB-UART utility

5

07-May-2013

USB-I2C Utility

6

08-May-2013

Danger Shield with Light Sensor Control

7

09-May-2013

Danger Shield with 7-segment display

8

10-May-2013

Danger Shield Buzzer of Doom

9

13-May-2013

Graphics LCD Display

10

14-May-2013

LCD - Rotating Cube Demo

11

15-May-2013

GLCD Paddle Game

12

16-May-2013

Pioneer Board Oscilloscope

13

17-May-2013

CapSense Button & LED Control with Bridge Control Panel

14

20-May-2013

What was the value? - LED Memory Example

15

21-May-2013

CapSense Proximity Detection

16

22-May-2013

Proximity Theremin

17

23-May-2013

2-Channel OScope with GraphicsLCD

18

24-May-2013

'Catch the Shells' Game with ColorLCD Shield

19

28-May-2013

LED Memory! Part Deux. Just Deux it!

20

29-May-2013

Starter Designs

21

30-May-2013

Fractional Frequency Synthesizer

22

31-May-2013

“Kill The Ghost” Game

23

03-Jun-2013

tinyprintf Example

24

04-Jun-2013

XBee Router Loopback Example

25

05-Jun-2013

XBee Direct IO

26

06-Jun-2013

XBee API RxTx Example

27

07-Jun-2013

XBee RGB CapSense Control

28

10-Jun-2013

“WiFi? Why Not!” Arduino WiFi Shield Example

29

11-Jun-2013

Bluetooth Home Automation System

30

12-Jun-2013

Bluetooth with GLCD

31

13-Jun-2013

Ethernet Shield

32

14-Jun-2013

More Relay!

33

17-Jun-2013

Sweet Music Everywhere! MIDI Shield

34

18-Jun-2013

Resistive Touch Example

35

19-Jun-2013

UART, I2C, and SPI Joystick Example

36

20-Jun-2013

What? I can use the PSoC 5LP too?

37

21-Jun-2013

PSoC With Friends! Word Scramble Game

38

24-Jun-2013

Ultrasonic Distance Measurement

39

25-Jun-2013

Two PWMs for the price of one

40

26-Jun-2013

Pioneer PnP Sensors

41

27-Jun-2013

Thermistor Example

42

28-Jun-2013

Hangman Game

43

01-Jul-2013

Rise of the Machines (Rolling Robot)

44

02-Jul-2013

Run Away Run Away! (Proximity Robot)

45

03-Jul-2013

Stepper Motor Example

46

05-Jul-2013

“Paint The Night” Accelerometer Example

47

08-Jul-2013

Obstacle Avoider Robot

48

09-Jul-2013

Walk The Line! Robot Example

49

11-Jul-2013

Android Device Controlled Robot

50

12-Jul-2013

SD Card Example

                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                  

S No

Date

Project Title

51

15-Jul-2013

Music Player

52

16-Jul-2013

Strike A Pose! Digital Camera

53

17-Jul-2013

PSoC Eye

54

18-Jul-2013

Custom Component 4x4 Keypad

55

19-Jul-2013

Parallel to Serial UDB Component

56

22-Jul-2013

Accelerometer Level

57

23-Jul-2013

Digital Audio From A Single Pin

58

24-Jul-2013

An Introduction to Processing

59

25-Jul-2013

But Wait There’s More! Single PWM with 3 Outputs

60

26-Jul-2013

PSoC 4 Mini-Billboard

61

29-Jul-2013

Nokia 5110 LCD Interface

62

30-Jul-2013

Ready…Set…GO! PSoC Stopwatch

63

31-Jul-2013

Some Like it Hot! PSoC Thermostat

64

01-Aug-2013

Workspace Organization using PSoC Theromostat

65

02-Aug-2013

New to PSoC or the Pioneer Kit? START HERE!

66

05-Aug-2013

LED Blinky Revisited

67

06-Aug-2013

PSoC 4 Getting Started Lab 1 (LED Blinky)

68

07-Aug-2013

PSoC 4 Getting Started Lab 2 (PWM LED)

69

08-Aug-2013

PSoC 4 Getting Started Lab 3 (CapSense UART)

70

09-Aug-2013

PSoC 4 Getting Started Lab 4 (ADC)

71

12-Aug-2013

Get Your Motor Runnin’!

72

13-Aug-2013

TFT Touchscreen Shield

73

14-Aug-2013

TFT Touchscreen Tic-Tac-Toe Game

74

15-Aug-2013

PSoC Creator Training 110

75

16-Aug-2013

PSoC Creator Training 111                                          

76

19-Aug-2013

PSoC Creator Training 112

77

20-Aug-2013

PSoC Creator Training 113

78

21-Aug-2013

PSoC Creator Training 210

79

22-Aug-2013

PSoC Creator Training 211

80

23-Aug-2013

PSoC Creator Training 212/213/214

81

26-Aug-2013

NFC/RFID Shield

82

27-Aug-2013

RFID Reader and Writer Project #2

83

28-Aug-2013

Raspberry Pi Integration

84

29-Aug-2013

State Machines in PSoC 4

85

30-Aug-2013

UART Bootloader in PSoC 4

86

03-Sep-2013

GPS Algorithm

87

04-Sep-2013

Gas Sensor Example

88

05-Sep-2013

Simulation of Gas Sensor Example

89

06-Sep-2013

GPS Example

90

09-Sep-2013

Comparator Example

91

10-Sep-2013

Infrared Remote Control

92

11-Sep-2013

Serial Communications Examples

93

12-Sep-2013

4 Channel Multiplexed Comparator

94

13-Sep-2013

Opamp Dynamic Gain

95

16-Sep-2013

Hibernate and Stop Power Modes

96

17-Sep-2013

P4 Light Sensor Project Design

97

18-Sep-2013

Rice Cooker

98

19-Sep-2013

Thermal Printer

99

20-Sep-2013

I2C Pass Though 'Smart Wire'

100

23-Sep-2013

PSoC 4 Time Square Billboard

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

I stumbled recently over a document (chapter 5.2 pg 28) that describes as a side-effect how to connect the Pioneer Kit to the PC displaying informations using the UART component. The "secret" are two (2) wires connecting the UART Rx and Tx to the on-board PSoC5LP Kit-programmer which then acts as an UART-to-USB bridge. On the PC-side I used the PuTTY program to display (and input) the data. In the description of the F-Ram Development Kit is a detailled procedure to set up the connection and hints where to download the needed terminal program. Remember that you do not need the F-Ram Kit, just put the two wires into the shown locations and all is well.

In short: drop a UART component on your sheet and use pins 0[4] and 0[5] for Rx and Tx
Connect external wires on the board between
J4 pin 1 ---Rx---- J8 pin 9
J4 Pin 2 ---Tx---- J8 pin 10

Download and install PuTTY

Bob

0 Likes