Seeing the same problem as: https://community.infineon.com/t5/PSoC-6/PSoC-6-BLE-Upgradable-Stack-Bootloader-compilation-build-er...
But the proposed solution is not a solution, because that setting is already OK:
I am seeing 2 issues:
1. Building app1 post step fails:
post_build_core0.bat creator .\CortexM0p\ARM_GCC_541\Debug Bootloader_BLE_Upgradable_Stack_App1 GCC
------------------------------------------
Post-build commands for Cortex-M0p core
------------------------------------------
C:\tmp\Bootloader_BLE_Upgradable_Stack_App1\Bootloader_BLE_Upgradable_Stack_App1.cydsn>"C:\Program Files (x86)\Cypress\PDL\3.0.1""\tools\win\elf\cymcuelftool.exe" --codeshare .\CortexM0p\ARM_GCC_541\Debug\Bootloader_BLE_Upgradable_Stack_App1.elf BLE_Symbols.txt GCC --output ..\Bootloader_BLE_Upgradable_Stack_App2.cydsn\BLE_core0_shared.s
Error opening file: ..\Bootloader_BLE_Upgradable_Stack_App2.cydsn\BLE_core0_shared.s
The command 'post_build_core0.bat' failed with exit code '1'.
However, this seems like an error that can ignored, since this output file should not exist yet. The instructions are quite clear: on P2: 2. Build the projects in the following order: App0, App1, and App2.
2. Building app 2 fails:
arm-none-eabi-gcc.exe -Wl,--start-group -o C:\tmp\Bootloader_BLE_Upgradable_Stack_App2\Bootloader_BLE_Upgradable_Stack_App2.cydsn\CortexM4\ARM_GCC_541\Debug\Bootloader_BLE_Upgradable_Stack_App2_link.elf .\CortexM4\ARM_GCC_541\Debug\startup_psoc63_cm4.o .\CortexM4\ARM_GCC_541\Debug\main_cm4.o .\CortexM4\ARM_GCC_541\Debug\system_psoc63_cm4.o .\CortexM4\ARM_GCC_541\Debug\bas.o .\CortexM4\ARM_GCC_541\Debug\debug.o .\CortexM4\ARM_GCC_541\Debug\hids.o .\CortexM4\ARM_GCC_541\Debug\scps.o .\CortexM4\ARM_GCC_541\Debug\host_main.o .\CortexM4\ARM_GCC_541\Debug\bond.o .\CortexM4\ARM_GCC_541\Debug\ias.o .\CortexM4\ARM_GCC_541\Debug\user_interface.o .\CortexM4\ARM_GCC_541\Debug\cy_ipc_config.o .\CortexM4\ARM_GCC_541\Debug\cyfitter_sysint_cfg.o .\CortexM4\ARM_GCC_541\Debug\cymetadata.o .\CortexM4\ARM_GCC_541\Debug\UART_DEB.o .\CortexM4\ARM_GCC_541\Debug\BLE.o .\CortexM4\ARM_GCC_541\Debug\BLE_config.o .\CortexM4\ARM_GCC_541\Debug\BLE_bas_config.o .\CortexM4\ARM_GCC_541\Debug\BLE_hids_config.o .\CortexM4\ARM_GCC_541\Debug\BLE_dis_config.o .\CortexM4\ARM_GCC_541\Debug\BLE_scps_config.o .\CortexM4\ARM_GCC_541\Debug\BLE_ias_config.o .\CortexM4\ARM_GCC_541\Debug\cy_sysint.o .\CortexM4\ARM_GCC_541\Debug\cy_ipc_drv.o .\CortexM4\ARM_GCC_541\Debug\cy_ipc_sema.o .\CortexM4\ARM_GCC_541\Debug\cy_ipc_pipe.o .\CortexM4\ARM_GCC_541\Debug\cy_sysclk.o .\CortexM4\ARM_GCC_541\Debug\cy_wdt.o .\CortexM4\ARM_GCC_541\Debug\cy_scb_common.o .\CortexM4\ARM_GCC_541\Debug\cy_scb_i2c.o .\CortexM4\ARM_GCC_541\Debug\cy_scb_ezi2c.o .\CortexM4\ARM_GCC_541\Debug\cy_scb_spi.o .\CortexM4\ARM_GCC_541\Debug\cy_scb_uart.o .\CortexM4\ARM_GCC_541\Debug\cy_efuse.o .\CortexM4\ARM_GCC_541\Debug\cy_flash.o .\CortexM4\ARM_GCC_541\Debug\cy_gpio.o .\CortexM4\ARM_GCC_541\Debug\cy_sysanalog.o .\CortexM4\ARM_GCC_541\Debug\cy_syspm.o .\CortexM4\ARM_GCC_541\Debug\cy_syslib.o .\CortexM4\ARM_GCC_541\Debug\cy_syslib_gcc.o .\CortexM4\ARM_GCC_541\Debug\cy_trigmux.o .\CortexM4\ARM_GCC_541\Debug\cy_systick.o .\CortexM4\ARM_GCC_541\Debug\cy_profile.o .\CortexM4\ARM_GCC_541\Debug\cy_prot.o .\CortexM4\ARM_GCC_541\Debug\cy_lvd.o .\CortexM4\ARM_GCC_541\Debug\cy_ble.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hal_int.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hal_pvt.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_gap.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_gatt.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_event_handler.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ancs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ans.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_aios.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_bas.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_bcs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_bls.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_bms.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_bts.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_cgms.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_cps.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_cscs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_cts.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_custom.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_dis.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ess.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_gls.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hids.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hps.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hrs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_hts.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ias.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ips.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_lls.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_lns.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_ndcs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_plxs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_pass.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_rscs.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_rtus.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_scps.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_tps.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_uds.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_wpts.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_wss.o .\CortexM4\ARM_GCC_541\Debug\cy_ble_clk.o .\CortexM4\ARM_GCC_541\Debug\cy_bootload.o .\CortexM4\ARM_GCC_541\Debug\BLE_core1_shared.o -mcpu=cortex-m4 -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -mthumb -L Generated_Source\PSoC6 -Wl,-Map,.\CortexM4\ARM_GCC_541\Debug/Bootloader_BLE_Upgradable_Stack_App2.map -T ./bootload_cm4.ld -specs=nano.specs -Wl,--gc-sections -g -ffunction-sections -Og -ffat-lto-objects -Wl,--end-group
./bootload_cm4.ld:243: non constant or forward reference address expression for section .cy_boot_ble_bss
The offending section is:
.cy_boot_ble_bss ABSOLUTE(__ble_core1_bss_start__) (NOLOAD):
{
*system_psoc63_cm4.o(.bss*)
*cy_ipc_sema.o(.bss*)
*cy_ipc_config.o(.bss*)
*cy_ipc_pipe.o(.bss*)
} > ram_ble_core1
@ShipingW_81 Can you look at this again?
Solved! Go to Solution.
I had this trouble at the same time. I solved it modifying the PATH of PDL version installed. I am using PSoC Creator v4.4 and PDL v3.1.5. The example code is the CE220960 ("DFU_BLE_Upgradable_Stack_App" project). You must edit the file post_build_core1.bat (in App0 and App2) and the file post_build_core0.bat (in App1).
Verifiying: Project>Build settings>
When Build App0 (Launcher)
CM4>Linker>Custom Linker Script>.\dfuCM4.ld
CM4>User commands>post_build_core1.bat
When Build App1 (Stack BLE and DFU boot)
CM4>Linker>Custom Linker Script>.\dfuCM0p.ld
CM4>User commands>post_build_core0.bat
CM4>Linker>Custom Linker Script>.\dfuCM4.ld
CM4>User commands>post_build_core1.bat
Note: Build App0 modify the BLE_core1_shared.s file to the Ap2 project. Click OK.
When Build Ap2 (User code)
CM4>Linker>Custom Linker Script>.\dfuCM4.ld
CM4>User commands>post_build_core1.bat
Note: The BLE_core1_shared.s is located in the Source files dir
I can solve it just today.
Attempting to archive the whole workspace produced no output. But here are the files for each app.
Environment:
PSoC Creator 4.2 (4.2.0.641)
PDL: 3.0.1
The problem seems to be the way the directories are structured when the Code Example wizard does it. There are several ways to do it, as a workspace or as independent projects. But none of them work without intervention. If you follow the default suggestions, it is always wrong.
The easiest way to create the whole workspace.
The rename the three apps it creates, removing the 01 suffixes.
When asked about renaming say Cancel.
Build the projects manually in this order: App0, App1, App2
Each will ask to upgrade the PDL, you also must press cancel.
I had this trouble at the same time. I solved it modifying the PATH of PDL version installed. I am using PSoC Creator v4.4 and PDL v3.1.5. The example code is the CE220960 ("DFU_BLE_Upgradable_Stack_App" project). You must edit the file post_build_core1.bat (in App0 and App2) and the file post_build_core0.bat (in App1).
Verifiying: Project>Build settings>
When Build App0 (Launcher)
CM4>Linker>Custom Linker Script>.\dfuCM4.ld
CM4>User commands>post_build_core1.bat
When Build App1 (Stack BLE and DFU boot)
CM4>Linker>Custom Linker Script>.\dfuCM0p.ld
CM4>User commands>post_build_core0.bat
CM4>Linker>Custom Linker Script>.\dfuCM4.ld
CM4>User commands>post_build_core1.bat
Note: Build App0 modify the BLE_core1_shared.s file to the Ap2 project. Click OK.
When Build Ap2 (User code)
CM4>Linker>Custom Linker Script>.\dfuCM4.ld
CM4>User commands>post_build_core1.bat
Note: The BLE_core1_shared.s is located in the Source files dir
I can solve it just today.