cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ Creator & Designer

Anonymous
Not applicable

In 2014, on the thread "PSoC Creator on Linux (or OSX) w/ or w/o wine", Scott Atkins said that a Linux version of PSoC Creator was "on the roadmap".

   

I am asking if that is still in the works and if we might see a PSoC Creator for Linux any time in the forseeable future?

   

If not, might there at least be a version that works well with WINE, please?

   

Thank you.

1 Solution
AnkitaS_51
Employee

PSOC Creator4.1  runs on these Operating System:

 Mac OS X El Capitan on VMware Fusion 8 running Windows 8.1
 Mac OS X El Capitan on Parallels Desktop 11 running Windows 10
 Ubuntu 15 Linux with Oracle VM VirtualBox running Windows 10

View solution in original post

0 Likes
3 Replies
AnkitaS_51
Employee

PSOC Creator4.1  runs on these Operating System:

 Mac OS X El Capitan on VMware Fusion 8 running Windows 8.1
 Mac OS X El Capitan on Parallels Desktop 11 running Windows 10
 Ubuntu 15 Linux with Oracle VM VirtualBox running Windows 10

View solution in original post

0 Likes
Anonymous
Not applicable

Does that mean Cypress no longer intends to make a PSoC Creator for Linux?

   

 

   

Does anyone know if it will run on Win 7 in Ubuntu 16.04 VBox?

   

 

   

Thank you.

mattl_01
Employee

Hi, unfortunately there are no plans for PSoC Creator to run on Linux.  😞

   

You may want to check out "Exporting a Design to Makefile" in the PSoC Creator help.  That may help some.

   

While we don't test on that specific Ubuntu/VBox combo, I see no reason why it wouldn't work.

   

--Matt

0 Likes