cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 6

yes_its_garen
New Contributor

Hi there! Hope you're doing well. I'm new to the whole Psoc 6 environment.

I am currently working on a project that requires me to transfer data acquired from the ADC and send it to an ESP32 via BLE. 

Till now I have finished the ADC part. And have done a lot of examples on the BLE (Glucose meter,  Heart rate monitor, Thermometer...).

I am now stuck making a BLE server that works. I am trying to use the CE222046_GATT_Out  example as previous forum responders have suggested, in order to create a custom service, but I am facing the following issue:

- After connecting to the GATT Out BLE server with NRF connect, I am getting disconnected when I try to enable notifications from the client side via the NRF connect app.

Also some important info:

- The CE222046_GATT_Out example is being used.

- I am using the CYBLE-416045-02 Psoc 6 prototyping board.

- I am using Psoc creator.

 

Can someone tell me what am I missing? It's been a while I'm stuck at this stage.

Thank you for your support 🙂

0 Likes
3 Replies
Yugandhar
Moderator
Moderator

Hello, 

Could you please share your project for checking at our end ?

Thanks,

P Yugandhar.

yes_its_garen
New Contributor

Project has been uploaded

0 Likes
Yugandhar
Moderator
Moderator

Hello,

Please refer to the attached Modified project. 

Please let me know if this helps.

Thanks,

P Yugandhar.

0 Likes
Top labels