PSoC™ 6 Forum Discussions
hello,
I am a beginner user
I am using CY8POROTO 063 BLE board , i want to Communicate between my PC and Board with my own C# App or CySmart App
forexample send a message form PC to board via bluetooth and vice versa
and i don't have CY5670 or 77 Dongle i am using CSR bluetooth dongle , Can i use this dongle with CySmart windows App?
what should i do?
Please help me!
thank u so much!
Show LessHi
i have a question
I'm working with the PSOC 6
I want to send text from my phone and receive it in PSoC?
for example send "Hello World" from my phone and Receive it in PSoC
then Send this text from PSoC To PC using UART
i think it should be very easy but i cant find any example for this project
i really need it please help me!
thanks
Show LessHello Cypress Community.
I am new to using PSoC 6 so please bear with me. I have been learning the PSoC 6 and I want to achieve a specific role.
The PSoC is running a GATT Server / GAP Peripheral, while there is an App running on Android as GATT Client / GAP Central.
The Client tries to connect to the PSoC, after connecting, it reads a Service called "STATUS" which is updated according the activities of the PSoC amd can be read only by the client. If the STATUS Characteristic is set to "StandBy", the client is able to enter different values in the application and Click on a button to send these values.
These values are configuration parameters (3 numeric values). which are required for the task that the PSoC does. According to the videos (which I learnt from), all the values that are controlled from the client are in the specified in the GATT Database as Services with available Characteristics and their values are updates (LED, Capsense). Now the question is, I want to receive these parameters, from the client app and parse them to do the required task. How do I receive values from the client after they click on the button on the app? Any available Code Snippets or Examples will be helpful.
Thank you
Show LessI have a question regarding the BLE Events.
Is it possible to process the BLE Stack events using Interrupts instead of putting Cy_BLE_ProcessEvents(); in a main loop that checks every time, so I an save the processor usage? Any example of that?
Show LessCY8CKIT-062 PSoC 6 BLE Pioneer Kit - Implement multi connection functionality using HID keyboard profile.
Problem Statement: We want to send keypress control to multiple devices simultaneously wherin kit will be connected to 4 devices and simulating any keypress on kit should be sent to all connected devices.
Tried:
- Downloaded set up CY8CKIT-062-BLE Complete Setup.
- In PSOC creator under code example section downloaded CE215121_BLE_HID_Keyboard sample code
- In Topdesign.cysch file changed maximum number of BLE connections to 4
- Kit starts advertising and connection to device1 is successful.
- In order to make it ready for 2nd connection we pressed SW2 button but it doesn’t start advertising hence device 2,3 and 4 are not able to see kit.
Kindly suggest us on how subsequent connections can be established. Also let us know if we are missing any major configuration that needs to be done.
Show LessI am trying to write a uint16 value to the a GATT Server attribute
The attribute is set to unit16 in the Service Configuration. However, this crashes the GATT DB as the PSoC module becomes unresponsive and I have to reset it.
if (CY_BLE_LEDSERV_TIMESTAMP_CHAR_HANDLE == writeReqParameter->handleValPair.attrHandle)
{
cy_stc_ble_gatt_handle_value_pair_t timeHandle;
timeHandle.attrHandle = CY_BLE_LEDSERV_TIMESTAMP_CHAR_HANDLE;
printf("0x%x\r\n", writeReqParameter->handleValPair.value.val[0]);
printf("0x%x\r\n", writeReqParameter->handleValPair.value.val[1]);
timeHandle.value.val[0] = writeReqParameter->handleValPair.value.val[0];
timeHandle.value.val[1] = writeReqParameter->handleValPair.value.val[1];
timeHandle.value.len = 2;
Cy_BLE_GATTS_WriteAttributeValueLocal(&timeHandle);
Cy_BLE_GATTS_WriteRsp(writeReqParameter->connHandle);
}
May I understand what am I doing wrong?
Thanks
Show LessHi, i can't find full list of all PSoC 6 MCU's
I find this side:
But here there are olny PSOC6ABLE mcu's(CY8C6xx6 and CY8C6xx7) I need list of PSOC6A2M and PSOC6A512K(CY8C6xx5, CY8C6xx8, CY8C6xxA) devices.
Where I can find that list?
Also I can find somewhere list of Silicon ID's all PSoC 6 devices?
Show LessWe have had some good results with the PSoC 6 WiFi prototyping board which is based on this module. The module is the CY8CMOD-062-4343W module, which is surface mounted on the proto board. I would like to use the module in our own boards but I can't find any news on the availability of the module or a roadmap of when it will be available.
Does anyone have any information on the availability of these modules? Just to stress again, I'm not seeking the prototyping boards, which are available, instead I want to purchase just the CY8CMOD-062-4343W module by its self to be integrated into new product designs.
Extra details:
Prototyping board containing the module: PSoC 6 Wi-Fi BT Prototyping Kit (CY8CPROTO-062-4343W)
On the photo on the product page the module is easy recognised in the middle on the left of the prototyping board. The module has the main PSoc6 processor and the module name is visible printed on it (upside down).
Show LessI need to layout a board using a CYBLE-416045-2 BLE module but i need to place my capsense buttons (5 of them) on top side of PCB and my components on the back side of PCB.
Can i do this in a way so the capsense will not be effected in a negative way. I would like some direction on how i can do this with as little adverse affects as possible. Could i get some support with this type of application please.
Scott
Show Less