PSoC™ 6 Forum Discussions
Hello there,
I want to create a interrupt botton in my project, using FreeRTOS, but the botton is not working. Someone can help me?
In some documents like this
PSoC6 MCU CY8C61x5, CY8C62x5 Architecture Technical Reference Manual PSoC 62 MCU.pdf
Clicking on the bookmarks does not work.
Show LessOn page 214 (section 19.2) https://www.cypress.com/file/385621/download it describes a default setting of the backup power domain to be Vddd if brown-out detect is enabled and no brown out event occurred. Looking at simplified schematics I see it explicitly connected to the Vdd pin or a separate power supply between 1.4 and 3.6 V. Could anything go wrong if the vbackup pin is only connected to a small capacitor and nothing else?
Show LessHi,
I'm using PSoC Creator 4.4 and PDL 3.1.3, and I have some variables that will be shared between CM0+ and CM4. I'm exploring ways to create a single linker script that contains specific sections that I can put these shared variables in.
I noticed there's a file named cycodeshareimport.scat and would like to know if I can use this to create my section, instead of having to put this section twice, once in M0 scatter file and the other in M4 scatter file?
Thanks!
Show LessI have an Psoc63 as BLE 5 central and three PSoC 4200 as BLE 4.2 peripheral. After a successful discovery from central using whitelist I try to connect to one of the three peripheral using his address. Unexpectedly the central was connected with a peripheral with different address!!!!! Also I try an unexisting address and again it was connected with a random peripheral with different address. Maybe the issue arise from the BLE 4.2 peripherals.
I will appreciate your help to this
Show Less
Hello, I am fairly new to the Cypress world. I am trying out the mtb-example-anycloud-ble-wifi-onboarding with my test kit CYW9P62S1-43438EVB-01. But I am getting below error upon building the application. I am using MoudusToolbox 2.2. I checked that 43438 is supported in the latest Bluetooth-freertos. Can I get some help please? Thanks in advanced!
Error message attached below:
------------------------------------------------
56 | #include "cycfg_system.h"
| ^~~~~~~~~~~~~~~~
compilation terminated.
make[1]: *** [../mtb_shared/core-make/latest-v1.X/make/core/build.mk:372: C:/Users/mingh/mtw/AnyCloud_Wi-Fi_Onboarding_Using_BLE/build/CYW9P62S1-43438EVB-01/Debug/wifi_task.o] Error 1
make[1]: *** Waiting for unfinished jobs....
In file included from ../mtb_shared/freertos/latest-v10.X/Source/include/FreeRTOS.h:56,
from ../mtb_shared/abstraction-rtos/latest-v1.X/source/COMPONENT_FREERTOS/cyabs_freertos_helpers.c:25:
./configs/FreeRTOSConfig.h:56:10: fatal error: cycfg_system.h: No such file or directory
56 | #include "cycfg_system.h"
| ^~~~~~~~~~~~~~~~
compilation terminated.
In file included from configs/app_platform_cfg.c:41:
configs/app_platform_cfg.h:46:10: fatal error: cycfg_pins.h: No such file or directory
46 | #include "cycfg_pins.h"
| ^~~~~~~~~~~~~~
compilation terminated.
make[1]: *** [../mtb_shared/core-make/latest-v1.X/make/core/build.mk:372: C:/Users/mingh/mtw/AnyCloud_Wi-Fi_Onboarding_Using_BLE/build/CYW9P62S1-43438EVB-01/Debug/configs/app_platform_cfg.o] Error 1
make[1]: *** [../mtb_shared/core-make/latest-v1.X/make/core/build.mk:382: C:/Users/mingh/mtw/AnyCloud_Wi-Fi_Onboarding_Using_BLE/build/CYW9P62S1-43438EVB-01/Debug/ext/mtb_shared/abstraction-rtos/latest-v1.X/source/COMPONENT_FREERTOS/cyabs_freertos_helpers.o] Error 1
In file included from ../mtb_shared/TARGET_CYW9P62S1-43438EVB-01/latest-v2.X/cybsp.h:28,
from main.c:43:
../mtb_shared/TARGET_CYW9P62S1-43438EVB-01/latest-v2.X/cybsp_types.h:25:10: fatal error: cycfg.h: No such file or directory
25 | #include "cycfg.h"
| ^~~~~~~~~
compilation terminated.
make[1]: *** [../mtb_shared/core-make/latest-v1.X/make/core/build.mk:372: C:/Users/mingh/mtw/AnyCloud_Wi-Fi_Onboarding_Using_BLE/build/CYW9P62S1-43438EVB-01/Debug/main.o] Error 1
In file included from ../mtb_shared/TARGET_CYW9P62S1-43438EVB-01/latest-v2.X/cybsp.h:28,
from ../mtb_shared/TARGET_CYW9P62S1-43438EVB-01/latest-v2.X/cybsp.c:29:
../mtb_shared/TARGET_CYW9P62S1-43438EVB-01/latest-v2.X/cybsp_types.h:25:10: fatal error: cycfg.h: No such file or directory
25 | #include "cycfg.h"
| ^~~~~~~~~
compilation terminated.
make[1]: *** [../mtb_shared/core-make/latest-v1.X/make/core/build.mk:382: C:/Users/mingh/mtw/AnyCloud_Wi-Fi_Onboarding_Using_BLE/build/CYW9P62S1-43438EVB-01/Debug/ext/mtb_shared/TARGET_CYW9P62S1-43438EVB-01/latest-v2.X/cybsp.o] Error 1
make: *** [../mtb_shared/core-make/latest-v1.X/make/core/main.mk:416: secondstage_build] Error 2
"C:/Users/mingh/ModusToolbox/tools_2.2/modus-shell/bin/make CY_MAKE_IDE=eclipse CY_MAKE_IDE_VERSION=2.2 CY_IDE_TOOLS_DIR=C:/Users/mingh/ModusToolbox/tools_2.2 -j8 all" terminated with exit code 2. Build might be incomplete.
11:27:41 Build Failed. 12 errors, 0 warnings. (took 13s.368ms)
Show LessHello all,
Does anyone know when a PSOC62 or PSOC63 variant with UDB and an SD Host controller will be available?
-=Eric Schumann
Hello.
I used PSoC 62S2 Wi-Fi BT Pioneer Kit.
Programming fails.
Could you please let us know a solution of this issue?
FW is hello world of Starter Application.
It is described as “Hello_World Program(KitProg3)” in Figure 2-10 of kit guide(002-28109).
But it is described as “Hello_World Program(KitProg3_MiniProg4)” in my tool.
Programming will fail even if mode is changed by SW3(MODE SELECT).
Best Regards.
Yutaka Matsubara
Show LessHello everyone, I bought a psoc CY8CPROTO-063-BLE and I don't know how to use this psoc with I2C-LCD. I wanna just a example like "Hello World", someone can help me?
Show Less