PSoC™ 6 Forum Discussions
Hi Sir,
客户目前在找不用添加外部时钟的MCU,也可以正常工作,请问PSOC4或者PSOC62,若是在PCB设计得时候,没有添加外部晶振的情况下,也可以正常工作吗?谢谢
Regards
Paddy
I want to use the TFT display and I2C sensors (e.g. BME280) to show the values. When the display is plugged in, the pins are assigned. How can you connect sensors and where do I get the voltage from? All pins are covered. Note: I used to work with the Arduino.
thanks to all
Show LessI use PSoC® 6 WiFi-BT Pioneer Kit (CY8CKIT-062-WiFi-BT), and IDE is ModusToolbox.
I want to use mbedtls and tcp, to develope a program using https client. Where can I find a runnable demo which have the similar featuure.
I have tried "Add Application" in ModusToolbox, but only find "AnyCloud_TCP_Client" and "AnyCloud_HTTPS_Server" demo. "AnyCloud_TCP_Client" just use tcp to connect a server without using mbedtls, and "AnyCloud_HTTPS_Server" don't have a sample code using connect interface with mbedtls.
I alse tried using "Library Manager" to add "HTTP-Client" library, but that demo can not be compiled correct, because of lack of "core_http_client.h" header file.
thanks a lot.
Show LessThis issue is with reference to mtb example psoc6 smartio sgpio target.
The SmartIO configurator does not carry the configuration applied to SmartIO during runtime. Can the run time configuration be updated, so that I need not decode the code in sgpio_target.c to understand and verify the SmartIO?
Best regards,
Sampath Kumar
Show LessI am using the B revision of the pioneer kit and therefore need to use PDL 3.0.1. Whenever I try to generate the ADC with this PDL I am unable to do so. How can I configure it to work with this PDL?
Show LessIs there any example code for using the ECC APIs? Mainly interested in the ECDSA processing specifically.
Thanks!
We are using a PSoC63 and transferring program over OTA into external memory.
External memory for bootloader - 512-Mbit (64mB) serial NOR flash, Quad SPI (QSPI) - S25FL512SAGMFI011.
One the bootloader is programmed into the external FLASH can you execute the bootloader ONLY out of the external FLASH?
This allows us to free-up FLASH memory on the P63 for application code.
Thanks
Show LessCY8CPROTO-062, -62S3, and -063 are marked as prototyping boards for PSOC 6. Looking into the BOM lists attached, all kits are listing CY8C5868LTI-LP039, which is a PSOC 5 family member. Are the BOM incorrect?
What MCU kits can I order to get a PSOC 6 chip?
Show LessI Designed this circuit based on the PSOC6 design guide.
Everything works well on this circuit except the BLE functionality. I made a FindMe program that works on the psoc 6 pioneer kit (powered by CY8C6347BZI-BLD53). However, when I migrate it onto my own design, it does not work. Specifically, the program crashes when I start any BLE functionality, such as calling Cy_BLE_Start(0). More specifically, when I call Cy_BLE_Start(0), other functions such as UART and blinky all stopped working. I tried to enter debug mode, but the play button for debugging is grayed out, and I can't even run the program in debugging mode. I have attached my FindMe project to this pose; any help will be greatly appreciated.
Show Less
I want to toggle between 40 pins using the AMUX block which would use the AMUX bus line in PSoC6 and connect the output of the mux to the Tx Pin in the cap sense module. However, I cannot find a simple/intuitive way of doing so - how do I connect the output of the Analog mux to the Capsense block in PSoC Creator? I have already tried to connect the output pin to the Tx pin in cap sense but it doesn't seem like there is a way to do that. Thanks.
Show Less