PSoC™ 6 Forum Discussions
hola comunidad! Me podría ayudar a saber y corregir el problema del por que me salen errores en la carpeta GeneratedSource al momento de configurar Bluetooth. Estoy usando eclipse IDE modustoolbox 3.1
Show LessWhere is the UCID of Infineon 9853 stored in 100TP
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/%E8%8B%B1%E9%A3%9E%E5%87%8C%E5%8A%A0%E5%AF%86/td-p/678687
Show LessHi,
We are using a CYB06445LQI-S3D42 device.
Starting with a default clock configuration worked well.
When we have tried to configure the system clocks according to our board design (we have an ECO), the BSP fails to initialize the clocks.
These are the parameters of the configurations. To note that exactly the same parameters work well on another project with exactly the same ECO but on PSOC63 (CY8C6347BZI).
The BSP fails in the clock initialization
Could you help me understand why and what to do?
Thanks
I'm failing to understand how systick timer ISR is being called when the project is generated by ModusToolbox.
Normally, when you setup the systick timer and enable its interrupt, Systick_Handler is called right from the interrupt vector. I can still see that Systick_Handler is the one in the startup_psoc6_02_cm4.s file. but looks like that it's not the actual function that services the systick interrupt. instead, Cy_SysTick_ServiceCallbacks function calls the functions that are registered by the user.
My question is that who and when and how the SysTick_Handler interrupt vector is changed? is it done by cortexM0 prebuild binary?
Thanks in advance.
Show Less
Hello~
I cannot download binary to my evkit board named CY8CKIT-062-WFI-BT after debugging.
So, I want to change the mode as recovery mode or bootloader mode with with pressing the some conbination buttons.
I cannot open CMSIS-DAP port IDE tool and it always display KITPROG3 update.
How can I handle this?
Many thanks
BRs
Show Less
Hello everyone, Happy New Year!! :))
I have a question for the PSoC 6, the board I'm using is the CY8CPROTO-063-BLE, and I want to make it work with low voltages, I know it can work with 3.3, 1.1 and 0.9 Volts, but I would like if there is possible to achieve it from the PSoC Creator program, as I know that soldering some pins is possible, but I'm wondering if there is a way without touching the hardware.
I learned that in PSoC Creator in the part of the System you can change in Operating conditions the Power mode from 1.1 to 0.9, even it says the VDD 3.3, do you think is possible to change that to 1.1 and 0.9 respectively and take this action as an undervoltage? Or is this not possible?
Thanks in advance,
Gio
Show LessHow to perform RF measurements of CYW43439 in CY8CPROTO-062S2-43439?
For an external antenna, I've removed the R15, added R11 and added an antenna connector at JI.
But on doing TX tests, transmitting packet engines, I'm not seeing any power in the power meter. Also associating the kit with another device the RSSI is also very poor(-91).
How to resolve this and perform RF measurements of CYW43439.
Show Less
Hi, i'm working with a CYPROTO-062-4343W PSoC6 Wi-Fi BT PROTOTYPING KIT and i'm trying to write a firmware to get capacitance and send the measurement through UART, but the code doesn't work on MODUS TOOLBOX, so i'm asking if there are any example codes for these type of operation?
Thanks in advance.
Here attached the code.
Show Less