Hi,
I am trying to port a PSoC 6 project from creator to modustoolbox and the last thing I need is to port to do is port our BLE OTA. The OTA is almost identical to the example project CE220960. I've added DFU into modus and changed the necessary function and variable names but I'm struggling with the linker scripts since as far as I can tell, there doesn't seem to be any examples for a BLE upgradable stack bootloader for modus. Basically what I'm looking for is any help with getting the linker files working for this port for the 3 projects (main app, launcher, stack). I put this project aside and just came back to it so apologies if I missed any information. Thank you in advance.
Solved! Go to Solution.
Hi @m_ost ,
There is a code example available for DFU_BLE in ModusToolbox which you can refer from the below link.
https://community.infineon.com/t5/AIROC-Bluetooth/MTB-PSoc6-BLE-OTA-Bootloader/m-p/330105#M1173
Regards,
Hi,
Can you send us the screenshot of the error you are facing while porting the code example so that we can assist you better.
Regards
Hi Alakananda,
Thank you for the reply, its not so much an error as not really knowing where to even start with the linker files. I did try just putting the PSoC creator linker files into modustoolbox but I was getting some errors which I've since forgotten as I reverted the linker files to their original state before temporarily putting the porting on hold. Although I do not remember what the errors were, in hindsight I believe it may have been because of BLE as our creator project has the ble set up in dual core mode, while the modustoolbox port has it in cm4 single core mode since I was having issues setting it up in dual core mode. What should my next step be? Should I:
Thank you,
Mike
To add to my question, I don't need to worry about the cm0 scripts since the modus project is in single core mode, correct? Looking at the Modus DFU example: https://github.com/Infineon/mtb-example-psoc6-dfu-basic I think that the answer is that I don't need to worry about them but I just want to make sure since I have very little knowledge when it comes to the linker scripts
After 2 days of messing with the linker files, I've gotten the 3 projects to build without errors and I use a post build to merge them together. After flashing the merged hex file, I seem to get nothing. I made an led light up at the very start of the launcher and it never even gets to that point. I am attaching the launcher and stack projects, and the linker/make files for our main app. I would really appreciate any help I can get with this from anyone.
Thank you,
Mike
Hi,
We are working with your project we will get back to you at the earliest.
Regards
Thank you, I am looking forward to your response
@Alakananda_BG , I am getting different advice here. It does not seem like porting from creator is a workable path.
https://community.infineon.com/t5/AIROC-Bluetooth/MTB-PSoc6-BLE-OTA-Bootloader/m-p/330105#M1173
Hi @m_ost ,
There is a code example available for DFU_BLE in ModusToolbox which you can refer from the below link.
https://community.infineon.com/t5/AIROC-Bluetooth/MTB-PSoc6-BLE-OTA-Bootloader/m-p/330105#M1173
Regards,