Hi Infineon Community,
I have CY8CKIT-062S2-43012 board. It has PSoC 6 MCU and CYW43012 IoT chipset. I am able to program and debug this board. But, I want to program / debug only CYW43012. There is on board JTAG PROG/DEBUG connector to 43XXX. Is this possible to program directly the CYW43012 chipset using JTAG.
If yes, what are the necessary steps should be taken to program/debug the only 43012 chipset?
Kindly see the J13 in below attached image, 43XXX PROG / DEBUG.
Solved! Go to Solution.
Hi @Vinayak,
It's not possible to program/debug the 43012 as standalone chip. We need to have a host processor connected to it.
Thank you
Best Regards
Raj Chaudhari
Hi @Vinayak,
It's not possible to program/debug the 43012 as standalone chip. We need to have a host processor connected to it.
Thank you
Best Regards
Raj Chaudhari
Thank you @Raj_JC for your response.
But, why there is JTAG connection for the 43012 on CY8CKIT-062S2-43012 board?
I found-out that, Wi-Fi JTAG interface is intended to be used by Cypress's internal teams only.