- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Device - CYBLE-416045-02
We are developing a BLE solution by using module CYBLE-416045-02 with several security features implemented by a external Trust-M through I2C communication. Besides, we use syspm to achieve power saving by making core m0+ and m4 go to deepsleep.
Unfortunately, we now bumping into a issue that i2c seems not working after m4 back to active. From LA displaying, we saw vcc and rst pins not pulled-high.
Anyone knows that any case can prevent I2C working in case of low power management?
Main flow
1. m0+ start itself and start BLE and m4 core.
2. m0+ going to deepsleep and process BLE events
3. m4 setup initialization (SAR, TCPWM, EEPROM, Trust-M & I2C, BLE)
4. ( main infinite loop ) m4 calls syspm to transit to deepSleep mode
5. ( main infinite loop ) m4 calls BLE process events
Hope anyone can help with some ideas or clues! Thanks!!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @okischuang ,
Could you please attach your project, if possible with only the I2C and low power mode part? We can have a look at the project and get back to you on what might be going wrong.
Also, you can refer to the PSoC 6 MCU Low-Power Modes and Power Reduction Techniques Appnote and the CE219881 - PSoC 6 MCU: Switching Between Power Modes code example which mentions the proper way to transition between low power mode and Active mode.
Best Regards
Ekta