cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 6

hoop4g
New Contributor II

Hello Team Cypress,

I am here to ask for a Cypress MCU that supports the following features.

The requirments are:
- The Cypress MCU will be used as Local Host MCU.
- The Cypress MCU must support Hardware Security Module (HSM) Multi2
- The Cypress MCU must support USB-IF (USB Interface)

Here is the block diagram where Cypress MCU is needed for the blue part of the blocks.

hoop4g_1-1629351354936.png

Would you share the best Cypress MCU part number with the features?

Thank you always.

Sincerely,
Ben

0 Likes
1 Solution
Ekta
Moderator
Moderator

Hi @hoop4g 

Could you please clarify the following points:

1. By Local Host MCU do you mean USB Host?

2. Whats functions do you want to be supported by the hardware security module (HSM)?

We have PSoC 64 Microcontrollers that seem to fit your requirement. This product line incorporates a full-speed USB device interface. The device can have up to eight endpoints. You can go through the product page and documentation provided in the link above and let us know if you have any further queries.

Thanks and RegardS
Ekta

 

View solution in original post

0 Likes
1 Reply
Ekta
Moderator
Moderator

Hi @hoop4g 

Could you please clarify the following points:

1. By Local Host MCU do you mean USB Host?

2. Whats functions do you want to be supported by the hardware security module (HSM)?

We have PSoC 64 Microcontrollers that seem to fit your requirement. This product line incorporates a full-speed USB device interface. The device can have up to eight endpoints. You can go through the product page and documentation provided in the link above and let us know if you have any further queries.

Thanks and RegardS
Ekta

 

View solution in original post

0 Likes
Top labels