cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 6 SDK

JaMi_334126
New Contributor II

Is there application software available to load onto a target PSoC to help RF agency (FCC for example) testing?

0 Likes
1 Solution
VenkataD_41
Moderator
Moderator

Hi,

If you are using PSoC 6 BLE, please find the attached project. This is a project similar to the PSoC 4 BLE’s integrated test code, where with a button press, the radio goes through different test modes required for FCC and most of RED testing.

Thanks

Ganesh

View solution in original post

3 Replies
VenkataD_41
Moderator
Moderator

Hi,

Please check the following KBA if you are looking for PSoC 4 BLE test firmware.

Test Firmware for PSoC®/PRoC™ BLE RF Certification – KBA220073

Thanks

Ganesh

VenkataD_41
Moderator
Moderator

Hi,

If you are using PSoC 6 BLE, please find the attached project. This is a project similar to the PSoC 4 BLE’s integrated test code, where with a button press, the radio goes through different test modes required for FCC and most of RED testing.

Thanks

Ganesh

View solution in original post

OscarC
New Contributor II

Hi all,

to avoid the possible problem in sending more than 104 packets with the TXP command, I suggest replacing this loop instead of the wait function

 

//CyDelayUs(num_packets * UNIT_PACKET_TX_TIMEOUT);
for(int32_t i=0;i < num_packets;i++)
{
  CyDelayUs(UNIT_PACKET_TX_TIMEOUT);
}

 

because the function CyDelayUs accepts an uint16 as a parameter.

Regards.

 

Oscar C.

 

0 Likes