cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

Hello,

I try to realize a synchronous demodulating of a signal modulated in 100khz.
I test the use of PSoc1. The use of " Modulation
Inputs " in a  SCC Block seem to allow it. But I do not how see routing this input with
PSoc designer 5.3.

0 Likes
2 Replies
Anonymous
Not applicable

The routing for modulation input of SC BLOCK (generic) user module is not shown in the device editor of PSoC Designer. You need to write into AMD_CR0 or AMD_CR1 register.

   

For more details about this register, please refer technical reference manual of the selected device. 

   

-Rajiv Badiger

0 Likes
ETRO_SSN583
Esteemed Contributor

In the TRM the section "23. Switched Capacitor PSoC Block" has the

   

registers you will need. Also AN2014 would be useful -

   

 

   

http://www.cypress.com/?rID=2899

   

 

   

Regards, Dana.

0 Likes