cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

Hi,

   

i have create 2 projects on psoc creator. In both use the 4 available opamp and was wondering if there is any way to switch between them without using the programmer?

   

Regards,

0 Likes
8 Replies
ETRO_SSN583
Esteemed Contributor

This might be of help -

   

 

   

http://www.cypress.com/documentation/application-notes/an73854-psoc-3-psoc-4-and-psoc-5lp-introducti...

   

 

   

Shows multiple applications usage.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

thanks dana.

   

I search on internet and i can't find examples for this.

   

It's more easy to find them..

   

Regards

0 Likes
Anonymous
Not applicable

hello dana, 

   

I'm use this example ( http://www.cypress.com/documentation/application-notes/an68272-psoc-3-psoc-4-and-psoc-5lp-uart-bootl...) and i can't send the files with "Uart Boolader  Host application".  The application block when i press "Bootload".

   

 

   

0 Likes
ETRO_SSN583
Esteemed Contributor

Did you follow the button press sequence show in the ap note, pages 16

   

on ?

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

i have test on psoc3. i didn´t have psoc4-

   

Regards,

0 Likes
ETRO_SSN583
Esteemed Contributor

Maybe file a CASE and give them your project archive -

   

 

   

To create a technical or issue case at Cypress -

   

 

   

www.cypress.com

   

“Support”

   

“Technical Support”

   

“Create a Case”

   

 

   

You have to be registered on Cypress web site first.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

Hi, I guess here the need of switching between two projects is re-use of opamps in different configuration. Note that, this can be achieved in single project itself. You can reroute PSoC analog component connections.

0 Likes
ETRO_SSN583
Esteemed Contributor

What are the two configurations you want for the OpAmps ? A schematic

   

of both configs would help.

   

 

   

Regards, Dana.

0 Likes