routing hardware to output pins
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
hi, 

   

help needed with routing internal hardware to specified pin.

   


I think I was overexcited by sypress advert - connect any pin to any hardware inside. But hopefully it is true and I just don't understand how to do internal routing. 

I want to leave all the connection as it is but connect pins 16 and 18 to my SAR ADC. I am sure I know how to do that - using analog multiplexer and then choose pin I need in software. but how to connect my TX module to pin 3? I couldn't find any way to do so.

   


thanks,
 

   

Oleg

0 Likes
2 Replies
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Pin 3 wants to take buss gloabalout3, which you have comitted to

   

Counter_10ms_base.

   

 

   

So you can share the pin using register writes to control the inputs to the

   

global buss, or if you do not need the 10 ms counter placed on the buss undo

   

the connection, or get a part with more pins.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

thank you very much, Dana! 

0 Likes