cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

I want to order a CY8CKIT-050B development kit.

   

please guide me about this kit

   

programming of this kit with USB can be easy  as using a MINIPROG3 ?

   

thanks

0 Likes
3 Replies
Bob_Marlowe
Expert II

Yes! Programming and debugging the  KIT-050 is quite the same as working with a MiniProg3. The kit has got two USB-connectors from which one is used to program and debug your project, while the other may used as an USB-connection for your your project, ie. an USBUART component.

   

Bob

0 Likes
ETRO_SSN583
Esteemed Contributor

From ( you can program via board USB or Miniprog3 interface )-

   

 

   

    

   

          http://www.cypress.com/?rID=51577

   

 

   

"The Kit-050 has an onboard programmer/debugger (Cypress USB chip based), which lets you program the PSoC 5 without connecting Miniprog3. This programmer debugs at a speed of 1.5mHz. The kit also allows the user to program and debug using the Miniprog3."

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 I would go as far as saying that programing it through the USB interface is actually easier than using a miniprog as all you do is connect the usb cable and run the programer/debuger no need to plug an aditional tool or making suer your connectors and voltage levels are right etc and even better it suppports most of the programing/debuging features of the miniprog 3.

0 Likes