cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable
        can you tell me the difference between CY8CKIT-050 and CY8CKIT-001 , which better and why ? i read both notes and i still confused which one to buy   
0 Likes
1 Solution
Anonymous
Not applicable
        Hi A.A welcome to the fantastic PSoC world.   
KIT-001 has all of PSoC devices PSoC5, PSoC3 even PSoC1.   
PSoC1 is a difference with others, that use PSoC Designer for IDE,   
Others are use PSoC Creator.   
On other hand, KIT-050 is dedicate PSoC5, using PSoC Creator for IDE.   
   
If I were you, I will buy KIT-050.   
Because, Creator has good features, and maybe familer to new comer.   
And KIT is simple rather than KIT-001.   
If you will become need PSoC1 device, think when its coming.   
   
Of course, you are rich man, buy both is good idea.   
Anyway, I have not neither of that.   
Thank you.   

View solution in original post

0 Likes
4 Replies
Anonymous
Not applicable
        Hi A.A welcome to the fantastic PSoC world.   
KIT-001 has all of PSoC devices PSoC5, PSoC3 even PSoC1.   
PSoC1 is a difference with others, that use PSoC Designer for IDE,   
Others are use PSoC Creator.   
On other hand, KIT-050 is dedicate PSoC5, using PSoC Creator for IDE.   
   
If I were you, I will buy KIT-050.   
Because, Creator has good features, and maybe familer to new comer.   
And KIT is simple rather than KIT-001.   
If you will become need PSoC1 device, think when its coming.   
   
Of course, you are rich man, buy both is good idea.   
Anyway, I have not neither of that.   
Thank you.   

View solution in original post

0 Likes
Anonymous
Not applicable

The CY8CKIT-050 kit is a PSOC5 dedicated kits and has onboard programmer/debugger. it is the most simple to use of all the kits but it only supports PSOC5.

   

The CY8CKIT-001 kit is more flexible. It supports 3 types of devices (PSOC 1 , 3 and 5LP). comes with plug-in mcu modules for the 3 types of devices and also includes a Miniprog3 programmer/debuger. To use it you have to plug-in one of the included mcu modules and the miniprog3 to the base board.

   

If you can aford it I would recommend the CY8CKIT-001 kit as it includes a miniprog3 that can be used to program external devices and supports all cypress devices.

Bob_Marlowe
Expert II

... and cypress told me there will be a PSoC4 processor module, so the Kit-001 will be able to support  *ALL* PSoCs.

   

I admit: I have got both Kits. When you start with the -50 kit there is no money thrown away when later on you decide to by a -001. As a mattert of fact: many projects include communication between two processor-boards via I2C, SPI or another protocol. So when owning two PSoC Kits you will be able to develop and test for those projects easily.

   

 

   

Bob

ETRO_SSN583
Esteemed Contributor

I do not know if this special is still in effect, check it out -

   

 

   

www.cypress.com/

   

 

   

http://www.cypress.com/?rID=37464

   

 

   

Regards, Dana.

0 Likes