cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

Hi

   

Please help me. How do i configure ADC for ecg? I want to use 14-bit adc. uC  is powered from 5 volts. Signal from instrumental amplifer have reference 2.5V.
How do I connect AGND and REF pin in psoc?

   

Best regards,

   

Waldi

0 Likes
1 Reply
ETRO_SSN583
Esteemed Contributor

If you look at startup page of PSOC Designer, there is a design catalog window with

   

several projects associated with ADCs, complete with code and settings.

   

 

   

These might help as well -

   

 

   

    

   

          

   

http://www.cypress.com/?rID=2843     AN2096

   

http://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&ved=0CCoQFjAA&url=http%3A%2F%2Fdigsys...     AN2239 (currently in revision)

   

 

   

Regards, Dana.

0 Likes