Hello, We have an application, in which, two trans-receiver are paired with unique address, master quering the slave for it's presence,...
Show More
Hello, We have an application, in which, two trans-receiver are paired with unique address, master quering the slave for it's presence, say every one second or so. If link is broken due to one of the device forming the pair move out of RF link range (150 ft. line of sight - outdoor, reduced inside the building) then alarm action is activated. We want to know, is it posiible to have 300 or more such pair operating inside same building or an hall area of 3000 sq. ft., with out interfering with each other's operation. Both Master and slave will be battery operated and carried by two different persons, accomping each other. Please suggest practical solution and applicability of CyFi in above application Regards Vinay Dand Mumbai electrocentre@vsnl.com Show Less
The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.