PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
Hi,
What is now the official version of silicon availability of PSoC5?
I know there is a few of them on evaluation kits, but the question is about the IC available to the masses.
I was promised samples about 6 months ago and nothing happened (had to use smth. else for the project)
The contest is a good way to make PSoC5 popular by showing what you can do with it, but if there is no silicon
what is the point of it?
Regards
Jan
Show LessI try make RFID reader project for CY8C3444LTI-110 device, but I can't find analog LPF filter (exist only digital filter) or modulator.
Do you have any ideas?
Best regards
Zbigniew Show Less
My project is to use a microcontroller in a device which can be controlled by the PC(windows) through usb, so the first requirement is to select a microcontroller which supports usb and based on 8051 core (PSoC-3). Also I have to write the .exe file (on PC) which will communicate with the microcontroller,recommended to use c++ or c as the programming language. So my question if you can help me with a ready made driver that can be used on the pc or integrated in the software to support communication with PSoC-3.I need also application notes on how to configure the PSoC-3 USB driver to be connected to the PC.
Thanks in advance
I'm developing a device that doesn't really fit into the common USB classes. I might be able to get most of the functions to work under the HID class, but some will still need to run under a more vendor-defined mode.
So I've been playing with the idea of using Vendor Defined commands on the control pipe. AN56377 has a good explanation of how to set up some basic vendor commands. However, it is missing some instruction. I want to be able to send and receive data payloads with the vendor commands. The App-note says that you have to use USBFS_1_InitControlWrite() or USBFS_1_InitControlRead() as needed, but gives no explanation of how to setup or retrieve that data payload. In fact, these functions, and USBFS_1_InitNoDataControlTransfer() are not even listed as part of the USBFS datasheet.
It seems to me that some of the advanced USB functionality has not been fully documented and/or the API has not been fully fleshed out with respect to vendor-defined usage. Is there a more complete version of the API listing available? Is there any more demo code that goes deeper into using the vendor functions of the USBFS component?
Show Lesshi is it possible to implement class f amplifier in psoc??
Hey guys,
I'm master's student and would like to join in contest, however I've few questions:
1. Until what time do I need to have design assets ready? or is it that I can submit it anytime until May?
2. Can I work in team with one of my friend?
3. Any general getting started you think is helpful
Thanks
Show LessHi,
I may be interested in participating in the challenge, but need some clarification on the resources.
If one makes it to the stage to receive a dev kit, what chip will it be, how much GPIO will the dev kit provide?
The design I anticpate may require up to 24 digital I/O pins, plus 8 Analog input pins, a couple of DAC outputs, and maybe a couple of event timer input pins. Maybe even another 13 I/O for a graphics LCD display. Will the dev kit be adequate to fulfill this?
Thanks,
Tony
Show Lesshello
now, I meet some issue:I measure the current:
when the voltage is above 3V, the current is about 10mA, but the voltage drops to 2.8V, the curren is 140mA, why? Do you meet this issue? pls give me some advise...
Show LessHi all,
I am trying to read the analog value output from a LM35 temperature sensor. I am reading the value received with the ADC, but I constantly get an offset of almost 1mV. This is problematic for me, since I am evaluating the PSoC devices for use in future products.
I am using a single ended delta sigma ADC with the following settings:
Conversion mode: Multi sample
Resolution: 16 bits
Conversion rate: 10 000 SPS
Input range: Vssa to Vdda (even though changing the range didn't do anything to my faulty reading)
Buffer gain: 1
Buffer mode: Rail to Rail
Reference: 3.2910V (As measured at Vdda)
I saw a demo where they got uV precision. Is it possible to get this kind of precision with this dev kit? How can I ensure precision when I produce my own PCBs?
Your help is appreciated.
Show LessHi,
I've been experimenting with a PSoC 3 'FirstTouch' eval kit. So far I am very pleased with it.
I am beginning to think about a serious application for a PSoC 3 chip, and thought I would circulate a few ideas here and see what the rest of the community think of it.
I'd like to build a universal IR (Infrared) receiver and decoder. One which can decode just about any common infra red remote control signal. The front end would be Vishay or Sharp Infrared receivers which demodulate the 36/38KHz signal.
I think I'd connect the output of the IR Receiver to a digital input pin.
So what would be best next? Can I implement an IR Signal decoder in hardware? Or should I simply generate an interrupt on the falling edge of the signal, then decode it all in software?
I've already done this several times in various projects, but using traditional micro-processors and doing it all in software. Mainly I just count deltas (the time the signal stays hi or low) and compare against a look up table, with a certain amount of jitter built in.
However in this new approach I wonder if it's possible to actually decode the IR signal and extract the control codes - preferably in hardware, or a combination of hardware/software. Any thoughts?
I already understand how to decode IR signals such as RC-5, RC-6 and so on, so I don't need references to 'understanding ir' - I'm more looking for any insight on the best approach to take to doing this on PSoC.
What would be best? A simple digital Input Pin, and ISR and software counters? Or some kind of digital input connected to a timer and shift register? How would that handle the preamble, and how could I detect different encoding schemes?
-Kenny
Show Less