PSoC™ 5, 3 & 1 Forum Discussions
I am using internal DAC in my program. I have set my DAC to 12 bit value. However, when I send DAC value over decimal 1038. My code goes to CyHalt reason 0. I am not sure why. Can someone help me how to resolve this issue.
Here is my DAC. I needed output to double, so I place a gain of 2 amplifier. Below is the set up for my DAC.
Show Less
Hello All,
I know chip availability has been haunting everyone as of late, but I was hoping to get some information around where the PSOC5LP is in its product lifecycle. Does anyone have any resources they can point me to that would indicate how long the PSOC5LP will be supported?
Thanks in advance.
Show LessHi,
I've developed three boards with a different pinout, let's say one board has an RTD in pins P0[3], P0[4], and P0[7] in one board. The other board has the same RTD, but is connected in pins P4[2], P4[3], and P4[4], is there a way to have two different TopDesigns in the same project and compile the project two times, disabling the page that I don't want to be compiled automatically? Maybe a script to select the files (but I don't know how to call PSOC creator from the terminal with specific files)?
Thanks
Show LessHi,
I have a weird issue with I2C (Master) generated code.
Sometimes the generated function 'I2C_MasterSendStart' fails (even if the bus is free) with error code 'I2C_MSTR_NOT_READY'.
I've found 'strange values' of the 'I2C_state' variable on such occasions. With 'strange values', I mean values (like, for instance, 0xD2) that, looking at the whole generated code, it cannot assume (memory corruption or am I missing something?).
Again, in such occasions, if I reset it to its default value (namely 'I2C_state = I2C_SM_IDLE;') then the I2C communication works again.
Could you please shed some light on this issue?
Show LessHi,
I am trying to load sample code to the evaluation board CY8CKIT-050B. However, the creator 4.2 gives compile error on all sample code.
Is there special version requirement for creator to compile sample code for this evaluation board?
Thanks,
Winston
Show LessWhat are the recommended PSoC 5-LP parts to replace PSoC 5 parts?
Specifically, for a design that used a PSoC 5, CY8C5468LTI-037, what is the correct PSoC 5 LP part that should replace it.
Generally, for any original PSoC 5 that was designed in, which PSoC 5 LP replaced it.
Greg
Show LessHi,
For PSoC 5LP I2C component, how to get error status of I2C_MasterReadByte() API? The function returns the byte read from slave. However, if something goes wrong, how can I get the error status?
Thanks,
Winston
Show LessNeed software for Windows 10 64-bit that can program PSoC 1 family, CY8C27443 parts. I plan to buy CY8CKIT-002 MiniProg3. I installed PSoC Programmer software 3.29.1 to make sure it will work with MiniProg3. But when I try to select the Device Family, then the specific device, I can't find anything close to CY8C27xxx.
What is the correct Windows software for use with MiniProg3 and CY8C27443?
Show LessKnown someone which polynomial code i must use for the CRC16 generator PSOC1 (CY8C29466)? The polynomial for the CRC16-IBM or CRC16/ARC is X16+X15+X2+1 I try with the polynomial 0xC002 and seed 0x0000 , but without a good result. The CRC16 generator is coupled with the same input of the Rx8 receiver and both data-inputs are inverted. The system works but i have a wrong CRC result. Have someone a suggestion ? Thanks!
Show LessIn this time of semiconductor shortage I am having difficulty finding a source of supply for the CY8C5888LT1-P097.
A sourcing company has come up with an alternative - the CY8C5868LT1-P097 which they say is identical except for the clock speed.
Looking for that device in the PS0C Creator library I can only find the CY8C5868LT1-P038 and -P039. Neither can I find it on the cypress/infineon website.
1. Does this device actually exist? Is it a cheap far-eastern copy? or is it just a CY8C58888LT1-P097 which did not quite meet the speed test?
2. If I get these devices, which device should I select for the build process? CY8C5888LT1-P097? CY8C5868LT1-P039? or CY8C5868LT1-P038?
3 what is the difference between the -P038, -P039 and P097?
Thank you
Peter
Show Less