PSoC™ 5, 3 & 1 Forum Discussions
Hi All,
PSoC 3 kits now ship with Production silicon. If you have bought a CY8CKIT-001 or a CY8CKIT-003, then your PSoC 3 kit may be in need of an upgrade.
Cypress Semiconductors would like to thank you for being loyal a Cypress Customer, and as an appreciation for your loyalty we invite you to upgrade your kit for free at www.cypress.com/go/psoc3kitupgrade
On the website you will find directions on how to upgrade your kit, if you have any questions you can e mail me at Jeffrey.musante@cypress.com
Thanks,
Jeff
Show LessHello,
I'm trying to create a very simple board and I need some help with people who already did this. I need a PCB board of 3.5"x2" where I can put 4 buttons at the top of the board and a slider down below. I need to be able to have proximity detection and be able to read the slider and the buttons (touch for the buttons and value for slider). (attached pdf with eagle demo board)
If you can provide the schematic and PCB board design in Eagle and quote me a price will be great. Again, I don't want to do it myself because I don't want to go thru the entire testing and guessing, etc. so please be gentle with the quote.
Thanks!
Show LessHi,
i need some rtos functionality for an embedded application. Through having keil c51 there is rtx51tiny included.
I already built a project using rtx51 but there seems to be problems with the timer 0 interrupt. Task switching os only done with explicitely calling os_switch_taks(). Self switching and os_wait does not seem to work.
I found, that there was an application note (AN64429.pdf) which couldn't be found anymore.
Would anyone b so kind to upload this file?
Thank
Show LessHello everybody:
I want to use my PSoC5 DVK which registers as a HID device in PC to communicate with MSPaint, and as you know MSPaint in windows7 surport multi-touch function, I want to use this function to test my touch based system, but i don't know how to achieve this testing function. Can you give me some suggestion?
Show LessIn working with the FTK, I would like to duplicate the onboard JTAG functionality provided by the CY7C68013A microcontroller.
Why are both SW0IO and SW0CK provided by USBIO (P15_6, P15_7) and PORT1 (P1_0, P1_1) attached to this microcontroller? Which of these two are being used for programming the PSOC5? Could someone with familiarity with the schematic for the FTK and PSOC5 line elaborate this a little further?
Thank you.
Show LessHi all,
With PSoC Creator 2.0, the following Development Kit projects will fail.
CY8CKIT-050 - LowPowerDemo
CY8CKIT-001, CY8CKIT-010 - Ex4_USB_HID
To get installer package with updated example projects, please visit the product webpage.
Show Less
Hi all,
With PSoC Creator 2.0, the following Development Kit projects will fail.
CY8CKIT-050 - LowPowerDemo
CY8CKIT-001, CY8CKIT-010 - Ex4_USB_HID
To get installer package with updated example projects, please visit the product webpage.
Show LessI am trying to build code for the Psoc5 that uses the itoa function from stdlib.h.
I have the #include <stdlib.h> at the beginning of main.c but It is not being included and I am getting errors related to
undefined references to itoa. Do I need to explicitly set the include path in the build settings? and if so where would they be located.
Thanks
Show LessCan I run a GPIO pin as output, open drain, drive low and attach an external pullup to 5V while the system is running 3.3V? All VDDIO is 3.3V.
Show LessI intend to use an external RAM with a PSoc3 chip. I find EMI component is available in the standard component library.
And it has got ADDRESS , DATA and CONTROL type of I/Os. There are total five(5) I/Os are given without any detail .
The standard controls required for such interface are CE,OE and WR. However, to my surprise I coundn't find any hint
about the usages of the 5 Control pins in the component data sheet. So, when I sit with the hardware design I am not sure about the pin assignments. And I don't find any example on EMI as well. Also , I am not sure about the software implementation of the EMI. Can I get some help on this issue?
Regards.
A.R.Bhattacharya.
Show Less