PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
I am facing problem with receiving multiple data bytes. I don't know whether the way i have implemented is correct or not.
I have enabled interrupt of SPIs as interrupt on RX_FIFO_NOT_EMPTY.
In the isr i read the no of. bytes received SPIS_ReadRxBufferSize and display the values on LCD directly.
Initially i had set buffer size of 4 and hence i was just able to get only 1 byte of data even on sending 3 bytes as no. of bytes SPIS_ReadRxBuffer was returning only 1(even datasheet says it provides 1).
So I changed to more than 4 bytes buffer. But still i am unable to receive the bytes.
Any solutions ??
Show LessI need to create a version of the quadrature decoder that has a true 24 or 32 bit counter.
The standard PSoC Creator install seems to be missing a project file so it can't be modified as if it were a "custom library".
Any help is appreciated,
Steven Show Less
I image could not create the firmware in psoс desinher in assembler for flashing LEDs. If someone has an example project with pictures or video tutorial on creating projects please please I will be very grateful. Excuse me please either something is not clear I from Ukraine and difficult for me to correspond to the English
Show LessSo I read the application note regard peak detection on the PSoC (AN60321) and the Peak and Hold method is exactly what I am looking for, only problem is I can't get it to work at a frequency faster then 4 MHz which it says is due to the mixer being used (The LO cannot exceed 4 MHz). I am trying to measure the peak voltage of a pulse that is about 3 microseconds in duration so I get about 12 samples per pulse (3 microseconds/250 nanoseconds).
Is there any way to get around the 4 MHz macimum LO, or is there an altogether better way to detect peaks at higher frequencies?
Show LessHi Everyone,
I got an error that has me stuck. My attachment shows the error pop up and my note explains how I got there.
Any help would be appreciated. Thanks TDGM
Show LessIn my project I want to stop the external crystal during low power mode and restart it again during the high power mode.
The crystal is for functioning of USB.
Can you tell the steps to be followed while changing the clock sources.I want to change the main clock from XTAL to IMO oscillator
Show LessHere is a much needed appnote to build a good design using PSOC3/5
http://www.cypress.com/?rID=43337
Show LessWhenever I call USBUART_Stop() even before starting the USB UART component that is USBUART _Start() the , I am seeing that the component doesn't even work.
I noticed that USBUART _CLK_Enable bit doesn't get set even if it is assigned 1.
You can reproduce this issue by opening the simple USBUART example project that comes with the creator and just call USBUART _Stop() before calling USBUART _Start() and then you can see thyat USBUART_Clk_Enable bit not set and also enumeration doesn't happen .
Can you tell me what goes wrong if i call Stop before even starting the component.
Show Less