PSoC™ 5, 3 & 1 Forum Discussions
Hello,
In CapSense CSD (PSoC3), Sensor Auto Reset is very useful, but too fast for my applications. Is there any way to change the time in which sensor baseline arrive to data value (from 5-10sec to 30 -60 sec)? In PSoC1 it was simple to tune this parameter.
Thanks
Nicola
Show Lesshi to all,
I am getting the error and unable to over come .can any suggest .
thanks
PRP
----------------------------------------------------------------------------------------------------------------------------------------------------------
Show Lessi'm in a dilemma whether to use the internal default ISR or a user defined one when my RX buffer size is greater tha 4 bytes and when i tried using the UART example project for PSOC3 it worked fine with the hyperterminal doesn't the same code apply to a RFID reader interfacing ?? when i tried using the same code my LCD wasn't displaying anything...what might be the problem ?? and when we set our buffer size 12 bytes ...when is the recieve interrupt actually generated after it recieves the first byte or after 12 bytes?? in need of urgent help
Show LessI have a condition where in after running the project for say 30hrs or so the project execution goes wierd. I suspect a stack overflow because , when i do attach to ruuning terget and do step by step execution the program execution is not fine. It is not doing sequential execution of code.
How to find out whether any stack overflow has occured or not and the reasons why stack overflow occurs?
Show LessIn a project , I have configured DMAs TD to transfer 3 bytes of data.
The source is uint8 Temp_Data[0], basically an array of "2" bytes and i am icrementing source address on transfer.
Now is there any problem if mysource is an array less than the no, of bytes to be transferred.
Show LessI was looking for building a board for PSoC3, the boards Cypress provides are high end boards not afforable for students.
What is the starting point i should look for building the board. Any documents will be helpful
Show LessGPIOs can provide only 4mA of current and sink 8mA. Can I connect multiple pins to generate a current of more than 4mA.
So, if i want a current of 20mA can I connect 5 pins together to provide this current???
And also when I require 20mA to be sinked can I connect 3 pins together to sink in the current??
Show LessI liked the Glucose Meter Demo video www.cypress.com/?rID=43800 but there is no reference design, schematics or project based on the video.
The video fairly describes the internal hardware and the prototype board but I'd love to have a look at schematics and the project to understand all calibration flow
BR,
Oleg
Show LessHow can i write some data from SRAM to buffer of SPI . Buffer here refers to FIFO . So once i write a value to this buffer then I can transmit data from this buffer.
And also if there is a SRAM buffer then writing some value from DMA (SRAM to SRAM) will it help???
Show Less