PSoC™ 5, 3 & 1 Forum Discussions
hi...
i am using PSoC3- cy8c38466, which consists of 64 KB flash memory to store my code......but, my project code is too big to fit into this 64 KB flash......
Actually my flash memory is almost full, but my project is not yet completed....still it may need approximately 10 KB......so, can anyone suggest the solution.......
Is it possible to interface memory externally, to store rest of my code........? If it is, please suggest the way to do it so that my code should not break
Thank you
Show Lessi want to connect 2.048V source to the negative input of ADC in the top design layout in Creator 2.1.which source shall i use?VDAC,battery or Vref?
Show LessHi,
Just wanted some info about the TIA available...as in PSOC Creator. I wanted to know the following, i'll be using a PSOC5 in a photodiode application:
Input Bias Current.
Input Voltage Noise (nV/sqrt(Hz) or any other units) as well as its noise spectrum.
Power consumption.
Thanks
Masab Ahmad
Show LessHi,
i am a newbie programmer using PSOC 3 . I want to send data to across the USB Comm Port . I have an CY8CKIT-030 PSoC® 3 Development Kit. Please guide me as i do not know how to proceed further. Any help would be appreciated and helpful
Hi!
I've burnt a simple program for counting pulses per second at input pin on a CY8C001 kit. The problem is that it picks up random counts sometimes even if the ground is secured at input (when i expect counts to be seen as '0'). The counter is back to its accuratekeep hitting the 'reset' switch time to time. can i schedule this 'reset' action in my firmware, maybe once after every 10 seconds ? is there any API call for this?
Show Less- I created a new project using CY8C29466.
- I placed a PGA on ACB00
- PGA input is set to AnalogColumn_InputMUX_0
- InputMUX is connected to P0[1]
- PGA Analog Bus is connected
- PGA Gain is 1
- PGA Reference is AGND
- Buf 0 is connected to Port0[3]
- P0[1] is supplied input voltage with a pot 0 - 5V
- P0[3] does not follow P0[1] but stays near 0V
Anyone have an idea how to solve this problem?
Show Less