PSoC™ 5, 3 & 1 Forum Discussions
I try to read counter register. I'm sure thatTimer_24 works.
in main loop
Timer24_ReadTimerSaveCV(&readTimer);
LCD_Position(1,1);
LCD_PrHexInt(readTimer);
but LCD shows me only 0000, I couldyn't find why.
Show LessI try to read counter register. I'm sure thatTimer_24 works.
in main loop
Timer24_ReadTimerSaveCV(&readTimer);
LCD_Position(1,1);
LCD_PrHexInt(readTimer);
but LCD shows me only 0000, I couldyn't find why.
Show LessHi,
I use CY8C29466 chip. It is passible to set two interrupt at the same time for timers ?
When I set interrupt I can only choose one of the option (attached image)
I will be grateful for response
Regards, Łukasz
Show LessHi,
I had CY3214-PSoCEVALUSB Board, and PSoc on this board CY8C24094 broke.
CY8C24094 is not available for production, so I couldn't buy it. Can I replace it with another chip ?
I will be grateful for response
Regards, Łukasz
The attached example project can be used as a reference to understand and get started with the USBFS APIs in PSoC. It contains the comments which details the use and significance of each API being used.
This project can be used with the Streamer application that is provided by Cypress along with Cypress SuiteUSB to find the throughput of the USBFS firmware.
Hi,
I'm developping an USB application using USB interface on PSoC 3. I'm performing a migration from Microchip PIC18F to PSoC.
I would like to know if it is possible to change EP1 diection while the apllication is running?
I would like to reuse some code from the PIC source code. I noticed that the endpoint is used in both direction.
Thank you!
Show LessI have connected SDA and SCL lines of MPU6050 to P12.1 and P12.0 of PSoC3 board. i need to display the raw values of oriantation along x, y ,z axes on character LCD that is on board. please give steps and most importantly the CODE !!! thank you...
Show LessI think I know the answer (from lookng at the data sheets etc.) but before I start to re-think my overall architecture:
Can a PSoC5(LP) provide USB Host (not necessarily OTG) capability itself or must I use a separate USB host chip?
I need to provide USB Audio host capability for a design (so I can plug in headphones, speakers etc.) and I'm trying to keep the part count down. I don't need hub capability. I know I can use the PSoC as a USB 'device'.
Thanks
Susan
Show Less