PSoC™ 5, 3 & 1 Forum Discussions
What will be the pin config for this ??????? Please guide. we are in the last stage of that. Please check whether it is the right GUI performance or not.
Show LessUSB_DWR_VDDD_OPERATION UNDECLARED
I am working with a cy8ckit-059 trying to write see some sensor values read through i2c. The code compiles fine and I can step through it in debug without error; however, in the "Locals" window that appears while in debug mode the local variables aren't listed. I would like to be able to see the values of the sensors I'm communicating with as i step through the code. Is this not something that I can do? Do I need to setup a connection to a teraterm window or something? Thanks in advance.
Show LessThe command 'arm -none -eabi-gcc.exe' failed with exit code
https://cordis.europa.eu/project/rcn/199923/en .Please replicate this one & Provide a Hex file & GUI(EXE) for 3rd iteration of the software & 3rd iteration of the device.
Show LessCan you Replicate this project & send me the actual HEX file for PSoc 5LP Prototyping Kit?? Send it to -p20210447@hyderabad.bits-pilani.ac.in
Show Lesshttps://www.duo.uio.no/bitstream/handle/10852/82665/5/Olav-Bjerke---masteroppgave.pdf .
Seeking help to reproduce this project. Each & every code is there Please help. It's required on an urgent basis.
Show LessI want to know if suppose PSoc 5LP board has been already loaded with the existing HEX file then again want to load a different HEX file into that. Then what will be the step to load a new hex file upon the existing hex file loaded PSoc 5LP?
Show LessHi All,
Recently w.r.t a project on which I am working, I need to create the binary file of PSoC5 from the generated .HEX file. While going through the community I found an Application Note : AN73054 (PSoC® 3 and PSoC 5LP Programming Using an External Microcontroller (HSSP)) which mentions that Cypress has already developed an application (C# Application Name: HexFileParser_Psoc3_5lp). Can someone help me on finding or guiding on how to get it?
Show Less