PSoC™ 5, 3 & 1 Forum Discussions
Hello all ,
i've created a project and i want to send it to a friend to check my desgin ,
the problem is if i just zip the whole project and try to send it via email
i get a security block becuse i am trying to send executable files ,
is there a way to create a minimal project via psoc creator and just sent this project
and then on the target machine to do a fresh build ?
thanks lampel
Show LessI have a launcher-only dual-image bootloader and a combination application that it boots. Within the combination application, I attempt to change the active image using Bootloadable_SetActiveApplication() call. The call fails. I traced the problem all the way to an SPC call failing within CySpcLoadRowFull(). I think the root of the problem is that SPC is not started, so calling CySpcStart() fixes the problem. I also tried calling CyFlash_Start() instead, but that one seems to hang in the while() loop.
There is no mention of having to do something to initialize flash anywhere in the Bootloader/Bootloadable documentation. As a matter of fact, the CySpcStart() call is barely mentioned at all when I search the website. I am using PSoC Creator 4.1 - did something change with regards to this?
Anyway, I have a workaround, but I think this needs clarification and at least a documentation change.
Show LessHi there
I would need to know how set the start bit on Uart V 2_.50.
I need to comunicate with a device which needs: 1start, 1 stop, 8 bit, no parity.
Thank you.
Show LessHello Every one,
I have a psoc5lp chip. I want to update the firmware remotely via spi communication through raspberry pi. In order to do this, I need to implement bootloader. My question is how i can programm it?
I have no idea how to do this.
I will look forward to your suggestions.
Regards
Show LessHi, I am trying to set up a USB MIDI device with 2 endpoints, one for midi in and one for midi out (Standard USB Midi Interface), but I have not succeeded , I'll Attach my project so you can give it a look
It has been a pain trying to configure this, so if anyone can lend me a hand, I'll really appreciate it.
Thanks!
Show LessI am reading the App Notes AN64846 and AN92239, with lots of hints about proximity detection, but don't see any examples for the 20x66 line. Is proximity too difficult for this part? I see the 1st Touch Starter kit uses the 21434 (did proximity but now out of production). What does it have that 20x66 doesn't?
Show Lessアニュラリングについてご教授ください。
ボタンにアニュラリングを空けて、ボタンの寄生容量を減らそうと考えております。
AN64846(CapSense入門)を確認すると、アニュラリングはLEDホール用に使用することを推奨しているように見えます。
LEDホール用ではなく、寄生容量を減らす目的でボタンに穴(アニュラリング)を空けることは推奨されますか?
Show Less
I want to read an array in flash that I previously written array.
The steps done are:
1. Write the array in emulated eprom with "Em_EEPROM_Write"
2.Turn off the power of the psoc
3. Turn on the power and read the array
In mode debugging this array is '0'.
It is because when you reprograming the psoc creator put all '0' in flash??
Regards
Show LessHi.
I have purchased a PSoC5 and I want to use the TIA (transimpedance amplifer). Though I can’t find any information about the noise spectrum (input-referred noise, 1/f etc). Is it possible to obtain these information ?
Best regards
Show Less