Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 5, 3 & 1 Forum Discussions

david-given
PSoC™ 5, 3 & 1
I've just released an open source project based around a CY8CKIT-059 (FluxEngine; it's a floppy disk drive controller). Currently I have to tell peopl... Show More
euggersh
PSoC™ 5, 3 & 1
I have a design with a PSoC 5LP and two CY8C9560C port expanders.  One of them has A0 grounded and the other one has it tied to +5V, which give I2C ad... Show More
amva_3752821
PSoC™ 5, 3 & 1
We are using CYCMBR3116 for development of touch panel switch for home automation.CS0 is used for proximity trace and other other sensors are used for... Show More
NaAm_1281831
PSoC™ 5, 3 & 1
Hi, I would like to use the USB port (not the THUMB Connector) on the Demo kit CY8CKIT-059, and so I have taken working code example  "CE195277_ADC_a... Show More
PaCo_972561
PSoC™ 5, 3 & 1
Hi - I'm having trouble getting the thermistor example (ThermistorCalc Example) to route.  The example come with the pins assigned.  That builds fine.... Show More
BrBr_1320441
PSoC™ 5, 3 & 1
I have developed firmware for a family of products that we sell, all targeting the PSoC 5LP, which can be configured to be run on one of a few differe... Show More
suto_2664507
PSoC™ 5, 3 & 1
user_13463998@Dear Sir,Regarding PSoC 5 LP and C language, it is still a beginner and I am in trouble because I can not do a full-scale program.I hope... Show More
maboc_3939291
PSoC™ 5, 3 & 1
Hello,I'm using a PSOC 5LP097 KitProg: CY8C5868LTI fo my project.I want to store data on a SD card and I'm using this document to help me :https://www.cypress.com/file/135136/download... Show More
PaCo_972561
PSoC™ 5, 3 & 1
It complains failed to route net "AmuxNose:AMux_1_CYAMUXSIDE_A".  I disabled all other components and it still can't route the AMUX.  It's now essent... Show More
MaWo_1214996
PSoC™ 5, 3 & 1
Hello,I want to use the timer component to get the speed of an motor signal.I have no UDBs left and also don't want to use interrupts.The signal from ... Show More
Forum Information

PSoC™ 5, 3 & 1

The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.