Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 5, 3 & 1 Forum Discussions

akac_3894371
PSoC™ 5, 3 & 1
Hi,,Good Evening,I'm working on PSoC1 CY8C22x45 MCU, and for induction applications testing the feedbacksignals, like voltage, current, IGBT temperatu... Show More
PeSi_1583586
PSoC™ 5, 3 & 1
I have a PSoC5LP application which includes  bootloader and bootloadable components. On power-up, the bootloader checks the state of a  pushbutton. If... Show More
MaWo_1214996
PSoC™ 5, 3 & 1
Hello,I have problems with the following code, writing and reading data to the EEPROM.I always get not the same read back as I was written to the EEPR... Show More
jagic_3937361
PSoC™ 5, 3 & 1
We are using PSoC Creator 4.1 and converted our test application to bootloadable.When we flash over JTAG either  app_1.hex or app_2.hex the bootloader... Show More
Anonymous
PSoC™ 5, 3 & 1
I am trying to get a UDB based timer to reset when it captures a value, but nothing that I have tried has worked. Please take a look at the attached s... Show More
mikuc_4021796
PSoC™ 5, 3 & 1
Hello,my effort was to create a simple USB-I2S device, 16b/48kHz, only for Tx data.I did it on the CY8CKIT-059 Usb Dev Board.I tried really hard, but ... Show More
absoc_3968316
PSoC™ 5, 3 & 1
Hello,
solved msg Solved
SampathS_11  Can you please help me to know what is communication distance of the Power Line Communication using CY3274 Development kit and what are t... Show More
NiNa_4043086
PSoC™ 5, 3 & 1
I would like to measure temperature on my system using a thermistor. Can I connect the Vhi and Vlow to Vdd and '0' internally on PSOC to save two GPIO... Show More
dahec_263886
PSoC™ 5, 3 & 1
I am using several CY8CKIT-059 's in my project. On one (my Master) I use the UART on the KitProg end. On the other 8 (Slaves), I do not need the UART... Show More
jatoc_3265626
PSoC™ 5, 3 & 1
I'll start off with what I'm trying to do: I have a MAX11200 ADC that I'm interfacing with via a SPI Master in full duplex mode (using a CY8C3866PVI-0... Show More
Forum Information

PSoC™ 5, 3 & 1

The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.