PSoC™ 5, 3 & 1 Forum Discussions
PSoC™ 5, 3 & 1
Hello. Does Cyprus provide generic drivers for the Cy7C637 chip for sending and receiving data with a USB transceiver? If not, i...
Show More
Hello.
Does Cyprus provide generic drivers for the Cy7C637 chip for sending and receiving data with a USB transceiver?
If not, is there clear documentation available to develop this?
Many thanks! Show Less
Does Cyprus provide generic drivers for the Cy7C637 chip for sending and receiving data with a USB transceiver?
If not, is there clear documentation available to develop this?
Many thanks! Show Less
PSoC™ 5, 3 & 1
I'm looking at the possibility of using Cyfi for our products. We want to use this wireless technology for communication between a remo...
Show More
I'm looking at the possibility of using Cyfi for our products.
We want to use this wireless technology for communication between a remote controller and several Light dimmer.
With one remote controller you will be able to dim / change colours of several light dimmer. (select the device and change it according to your wishes)
Is it possible to use multiple remotes to controll all light dimmers?
Because you Bind a Hub (remote controller) with a node (light dimmer) my understanding is dat you can only controll the light dimmer with the remote which was used for binding.
Are there any solutions to use multiple remotes?
Are there any "Cyfi modules" available which can be plugged onto our pcb.
(just like you have the WUSB pre made modules)
This will save us a lot of design time. (we do not have to care about pcb layout)
If yes; are these modules available as samples?
Thanks, BR,
Jasper Show Less
We want to use this wireless technology for communication between a remote controller and several Light dimmer.
With one remote controller you will be able to dim / change colours of several light dimmer. (select the device and change it according to your wishes)
Is it possible to use multiple remotes to controll all light dimmers?
Because you Bind a Hub (remote controller) with a node (light dimmer) my understanding is dat you can only controll the light dimmer with the remote which was used for binding.
Are there any solutions to use multiple remotes?
Are there any "Cyfi modules" available which can be plugged onto our pcb.
(just like you have the WUSB pre made modules)
This will save us a lot of design time. (we do not have to care about pcb layout)
If yes; are these modules available as samples?
Thanks, BR,
Jasper Show Less
PSoC™ 5, 3 & 1
Hello I have to design a filter at 100 HZ PSOC using C language, can be FIR. I should not use the libraries firfilters.ho iirfilters.h. ...
Show More
Hello
I have to design a filter at 100 HZ PSOC using C language, can be FIR. I should not use the libraries firfilters.ho iirfilters.h.
I have coefficients matlab, but not to make the algorithm in C to filter a signal.
I filter the signal from an ADC.
thanks. Show Less
I have to design a filter at 100 HZ PSOC using C language, can be FIR. I should not use the libraries firfilters.ho iirfilters.h.
I have coefficients matlab, but not to make the algorithm in C to filter a signal.
I filter the signal from an ADC.
thanks. Show Less
PSoC™ 5, 3 & 1
PSoC™ 5, 3 & 1
HI We just use the chip cyrf69103 to design. we use the IDE 'psoc designer5.0' for this project. We added the CYFISPI module to our project...
Show More
HI
We just use the chip cyrf69103 to design. we use the IDE 'psoc designer5.0' for this project. We added the CYFISPI module to our project .But it can not work.The firmware can not retrieve an nonzero number after call the 'CYFISPI_Start()' function .
I want to know if the psoc designer 5.0 has some bug on the CYRF69103. And how we shoud use the CYFISPI module . Show Less
We just use the chip cyrf69103 to design. we use the IDE 'psoc designer5.0' for this project. We added the CYFISPI module to our project .But it can not work.The firmware can not retrieve an nonzero number after call the 'CYFISPI_Start()' function .
I want to know if the psoc designer 5.0 has some bug on the CYRF69103. And how we shoud use the CYFISPI module . Show Less
PSoC™ 5, 3 & 1
Hello. I am an undergraduate student working on a project to create a wireless remote control. My professor has given me a CY3653 developme...
Show More
Hello.
I am an undergraduate student working on a project to create a wireless remote control. My professor has given me a CY3653 development kit. We are planning to use the Wierless USB module to for the remote . The data to be transmitted will be sent to the Wireless USB module via a serial RS232 connection.
Before moving on to the RS232 examples, I decided to try out the other examples.
The WUSB modules came pre programmed with the protocol tutorial which worked perfectly. I programmed them with the radio tutorial program, it also worked fine.(I am using PSoc Designer v4.4 with the HiTEC Lite compiler).The problems started when I tried to program the protocol tutorials and the RS232 Master- Slave programs.
But the to modules are unable to connect with each other.
Since the radio tutorial is working perfectly fine, there is no problem with the software.
Can someone please advise me on this issue.
-Arnav Show Less
I am an undergraduate student working on a project to create a wireless remote control. My professor has given me a CY3653 development kit. We are planning to use the Wierless USB module to for the remote . The data to be transmitted will be sent to the Wireless USB module via a serial RS232 connection.
Before moving on to the RS232 examples, I decided to try out the other examples.
The WUSB modules came pre programmed with the protocol tutorial which worked perfectly. I programmed them with the radio tutorial program, it also worked fine.(I am using PSoc Designer v4.4 with the HiTEC Lite compiler).The problems started when I tried to program the protocol tutorials and the RS232 Master- Slave programs.
But the to modules are unable to connect with each other.
Since the radio tutorial is working perfectly fine, there is no problem with the software.
Can someone please advise me on this issue.
-Arnav Show Less
PSoC™ 5, 3 & 1
I am considering using a PSoC device as part of an instrumentation system, but am worried that the amplifier ac specs may not be up to the job...
Show More
I am considering using a PSoC device as part of an instrumentation system, but am worried that the amplifier ac specs may not be up to the job. I need an instrumentation amp with gain of about 20-50, low bandwidth (up to 50kHz GBW) and low input noise (<5uV). The INSAMP quotes 0.75MHz GBW at 5V and a noise voltage input of about 100nV/rtHz, which would yield an input noise of 12uV at G=50. This is too high. Has anyone obtained actual noise figures for their similar designs please?
Show Less
PSoC™ 5, 3 & 1
Hello, We have an application, in which, two trans-receiver are paired with unique address, master quering the slave for it's presence,...
Show More
Hello,
We have an application, in which, two trans-receiver are paired with unique address, master quering the slave for it's presence, say every one second or so. If link is broken due to one of the device forming the pair move out of RF link range (150 ft. line of sight - outdoor, reduced inside the building) then alarm action is activated.
We want to know, is it posiible to have 300 or more such pair operating inside same building or an hall area of 3000 sq. ft., with out interfering with each other's operation.
Both Master and slave will be battery operated and carried by two different persons, accomping each other.
Please suggest practical solution and applicability of CyFi in above application
Regards
Vinay Dand
Mumbai
electrocentre@vsnl.com
Show Less
We have an application, in which, two trans-receiver are paired with unique address, master quering the slave for it's presence, say every one second or so. If link is broken due to one of the device forming the pair move out of RF link range (150 ft. line of sight - outdoor, reduced inside the building) then alarm action is activated.
We want to know, is it posiible to have 300 or more such pair operating inside same building or an hall area of 3000 sq. ft., with out interfering with each other's operation.
Both Master and slave will be battery operated and carried by two different persons, accomping each other.
Please suggest practical solution and applicability of CyFi in above application
Regards
Vinay Dand
Mumbai
electrocentre@vsnl.com
Show Less
- « Previous
- Next »