- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Greetings to All:
I am trying to reduce the ppm number on the 5LP. I have enabled the USB tab in the clock settings and have got a clock running at 1250ppm. I was hoping to attach an external crystal with some capacitors and use them to create a more accurate clock.
I was hoping to use a watch crystal with 20ppm. This is desirable as I am looking to microsecond timers that would be accurate.
Can I use the watch crystal, create and use a clock based off this at 24Mhz?
I am trying to locate documentation on this and my searches do not amount to any thing.
Help is appreciated, regards.
Ken.
Solved! Go to Solution.
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I'm sorry hearing that the USB Clock of 5LP does not have enough accuracy.
I tried with CY8CKIT-059. (5LP)
I'm afraid that there is no path from XTAL 32kHz to Master Clock.
The XTAL needs to be 4MHz ~ 25MHz.
Then I tried with CY8CKIT-044 (4200M)
If I set wco (32kHz) with 20PPM accuracy
We can trim IMO with WCO, so that IMO accuracy is +/- 0.2%
moto