cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

Hello,

   

I am a beginner.

   

I have a project but...

   

Where are PGA and ADC at System-level?

   

I know how to use them at Chip-level.

   

But my new project need them...

   

If not, how to make them?

   

Thank you~

0 Likes
15 Replies
rola_264706
Honored Contributor II

What do you mean system level? Do you mean at the chip level or assembly level in the program?

0 Likes
Anonymous
Not applicable

I add a file... Thank you~

0 Likes
Bob_Marlowe
Expert II

Welcome in the forum.

   

Drag and drop the components you need on the TopDesign view and configure them as you need.

   

Use the option to show the datasheet for the components to see how to access them in code.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

I know drag and drop but...

   

I add a file...

   

Please~

   

Thank you~

0 Likes
HeLi_263931
Honored Contributor II

Can you describe in a little bit more detail what you problem is? Normally you open the schematic for your project, add the required components to it, configure and wire them. Then you create your source files (or open main.c), include project.h at the top and call the needed APIs for the components.

0 Likes
Anonymous
Not applicable

I have a picture to describe...

   

Can you see it?

   

Please~

   

Thank you~

0 Likes
Bob_Marlowe
Expert II

When you do not see the picture, we will not see it either.

   

 

   

Bob

0 Likes
Anonymous
Not applicable
        Well... I can see a link, that can download the picture at my top article... I add it again. Can you see it now? Thank you.   

0 Likes
Bob_Marlowe
Expert II

The software for PSoC1 in your picture is obsolete for more than 4 years. You are posting here in a PSoC5 forum which is a completely different device.

   

Can you please elaborate and tell us what you want to do.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

I have a photodiode because I need "light intensity".
I have try it from https://www.youtube.com/watch?v=XhJxlZkFf7s

   

But I want the same one at System Level.

   

Q2 is my new picture.

   

1.There is my project block diagram.
2.This is  PSoC 5.0.
3.I can’t find components to drog and drop.  (PD.PGA.ADC) 

   

Q: Where are them or how can I do?

   

Thank you~

   

   

0 Likes
Bob_Marlowe
Expert II

What you have got is a PSoC1. The program you are using is PSoC Designer 5.0 (latest version is 5.4) There is no "System Level" for the design any more.

   

You are posting in a PSoC5 forum which is a completely different chip compared to a PSoC1 and uses completely different software.

   

I would like to give you the following advice:

   

Get a CY8CKIT-059 PSoC5 Prototyping Kit or at least a CY8CKIT-043 PSoC4-M Prototyping Kit. What you get more is

   
        
  • SRam
  •     
  • Flash
  •     
  • Debugging capabilities
  •     
  • Modern ARM M3 or M0 CPU core
  •     
  • ~100 ready-to-use components
  •     
  • Reasonable price
  •    
   

 

   

Bob

0 Likes
Anonymous
Not applicable

Hi Bob

   

I have the same issue with glacialionepoch_1604421.

   

Actually, Psoc 5.0 has system level interface.

   

I think system level is more friendly than chip level, just a little issue --> I often can't find component that I need .

0 Likes
Bob_Marlowe
Expert II

Welcome in the forum, Charlie!

   

As I stated before: Cypress is at version 5.4 with the Designer software and the "System level" has been abandoned due to severe errors some years ago. And just to keep it right: You are not talking about PSoC 5.0, you are talking about PSoC Designer 5.0.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Hi Bob

   

Thanks for your answer. 

   

Yes, I mean Psoc Designer 5.0, Sorry for misread your reply.

   

As your words, I think  "system level" were abandoned because some errors in this interface. Am I right??

   

One more question. Do you recommend  I use chip level interface even I use Psoc Designer 5.0??

0 Likes
Bob_Marlowe
Expert II

When you are a beginner I would suggest you not to use PSoC1. The reason is: Debugging the code is only possible with additional hardware (ICE Box). This can make the development of more complex applications very difficult. Way out could be for you to get a CY8CKIT-059 PSoC5 Prototyping Kit or at least a CY8CKIT-043 PSoC4-M Prototyping Kit.

   

You will have to use C-language to program any of the PSoCs. Furthermore: Use the actual IDE which is Designer 5.4 for PSoC1 and Creator 3.3 for PSoC3,4,and 5.

   

 

   

Bob

0 Likes